LS1046A thermal design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A thermal design

Jump to solution
817 Views
Nareshvarikuntla
Contributor III

Dear NXP,

I would like to have custom made heat sink attached to LS1046A. What is the maximum pressure LS1046A can able to withstand. How much contact pressure LS1046A needed for good thermal design.

I will be happy if you can share other relevant thermal design information.

Regards,

Naresh V.

Tags (2)
0 Kudos
1 Solution
806 Views
Nareshvarikuntla
Contributor III

Thanks for the response.

View solution in original post

0 Kudos
2 Replies
807 Views
Nareshvarikuntla
Contributor III

Thanks for the response.

0 Kudos
810 Views
andrei_skok
NXP Employee
NXP Employee

Please look at the LS1046 Datasheet https://www.nxp.com/docs/en/data-sheet/LS1046A.pdf, chapter 6.3 Thermal management information.

Here you can find our recommendations for thermal design.

"The heat sink should be attached to the printed-circuit board with the spring force centered over the die. This spring force should not exceed 15 pounds force (65 N)."

0 Kudos