已解决! 转到解答。
Please refer to the following update from the AE team.
I did a presentation for Fiberhome a while back. Look at slide #37. What is your IF_MODE?
For RGMII, the TX is source synchronous (we send the clk with the data).. The speed selection in the MAC will control the dividers to give the correct freq on TX.
For RX, you have to supply the correct freq to the rx clk (2.5MHz, 25MHz, or 125HMz).
Please refer to the following update from the AE team.
I did a presentation for Fiberhome a while back. Look at slide #37. What is your IF_MODE?
For RGMII, the TX is source synchronous (we send the clk with the data).. The speed selection in the MAC will control the dividers to give the correct freq on TX.
For RX, you have to supply the correct freq to the rx clk (2.5MHz, 25MHz, or 125HMz).
Hi Yiping,
thank your for help. The document is very useful.
IF_MODE register content is 0x600a0000
bit 0-bit 15 = 0x0000
bit 16 = 0 => ena
bit 17 = 1 => ssp
bit 18 = 0 => ssp
bit 19 = 1
bit 20 = 0
bit 21 = 0
bit 22 = 0
bit 23 = 0
bit 24 = 0
bit 25 = 0
bit 26 = 0
bit 27 = 0
bit 28 = 0
bit 29 = 1 => rg
bit 30 = 1 => if_mode
bit 31 = 0 => if_mode
Best regards
Brahim
Hi Yiping,
from the document LS1043ADPAARM 6.4.3.3.1 Interface Mode Register (IF_MODE) table 6-87. IF_MODE Field Description I read:
17–18 SSP
• 00 - 100 Mbps RGMII (valid only if ENA=0)
• 01 - 10 Mbps RGMII (valid only if ENA=0)
• 10 - 1 Gbps RGMII (valid only if ENA=0)
• 11 - Reserved
for 1Gbps bit 17 = 1 and bit 18 = 0 or is it the contrary ?
I'm not sure of the higher significant bit in the table.
30–31 IFMODE
• 00 - 10G interface mode
• 01 - MII mode
• 10 - GMII mode (also for RGMII)
• 11 - Reserved
for GMII mode (also RGMII) bit 30 = 1 and bit 31 = 0 or is it the contrary ?
I'm not sure of the higher significant bit in the table.
Best regards
Bahi
The interface with if_mode register is big endian. So I swapped the bit0-15 with the bit16-31 and now the frequency is OK (EC1_GTX_CLK output is 125 MHz):
bit 31-bit 16 = 0x0000
bit 15 = 0 => ena
bit 14 = 1 => ssp
bit 13 = 0 => ssp
bit 12 = 1
bit 11 = 0
bit 10 = 0
bit 9 = 0
bit 8 = 0
bit 7 = 0
bit 6 = 0
bit 5 = 0
bit 4 = 0
bit 3 = 0
bit 2 = 1 => rg
bit 1 = 1 => if_mode
bit 0 = 0 => if_mode
u32 value is 0x00005006
Thank you for your help.
Best regards
Bahi