LS1028A JTAG Connectivity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A JTAG Connectivity

1,124件の閲覧回数
Sathian
Contributor II

We have custom based LS1028A board and trying to halt the processor via JTAG. 

We could able to do "halt" in EVM(Attached image) but not in custom board, What could be the problem and solution ?

0 件の賞賛
1 返信

1,117件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which exactly DUT board is in question?

Is POR behaviour of the reset signals on the DUT board similar to shown in the "Figure 6. Power-On Reset Sequence" in the QorIQ LS1028A Reference Manual?

Is the DUT board capable to boot?

Please confirm that JTAG interface is implemented as described in the AN12028 - QorIQ LS1028A Design Checklist, 5.20 JTAG pin termination recommendations.

Is TRST_B asserted during power-on reset flow?

 

0 件の賞賛