I am planing to make an evaluation board for MML09212H.
could you please help me find gerber file or a layout to start working on?
The input and output return loss is very critical for me, I just wondering for frequency 400MHz and 900Mhz how may I get a better Return loss? which matching circuits would help me to get improvement of at least 3dB on the return loss?
Please, S-parameters and DXF layout files of the designs are provided on the product summary page:
Reference designs from the datasheet provides good enough matching. Actually, it is possible to improve narrowband matching in expense of the bandwidth.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------