JN5189 wakeup time from sleep

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5189 wakeup time from sleep

1,235件の閲覧回数
talhamir49
Contributor III

Hello 

I'm using the JN-5189 DK with the example JN-AN-1246, everything is working good but I'm facing a problem that when my device wakes up from sleep it took 60ms to wake up and consume 3 to 4 mA current.

cd1d9f20-ee34-4563-b197-58bda49f2d74.jpg

 

Attached is the photo of the oscilloscope showing the sensor time taken after wakeup and current consumption.

I'm at the end of the project and I need to minimize the size of the pulse so it can drain the minimum current.

kindly help me out.

 

Thank You 

Regards Talha

0 件の賞賛
返信
2 返答(返信)

1,221件の閲覧回数
talhamir49
Contributor III

Hi,

When the MCU wakes up none of the peripherals are reactive as before going to sleep I turn off all the peripherals. No other device is connected.

0 件の賞賛
返信

1,224件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

When the mcu wakes up, what peripheral are working? Do you close the console print? Do you insert any other device into the arduino connector?

0 件の賞賛
返信