JFET Spice models

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,315件の閲覧回数
ucetnahranie
Contributor I

Hi, 

I would like to ask, whether it´s possible (and if so, where) to get Spice models for following JFET transistors:

BFR31

BF556A

BF861A

1 解決策
1,921件の閲覧回数
LPP
NXP Employee
NXP Employee

I found these definitions:

*PHILIPS SEMICONDUCTORS        Version: 1.0
*Filename: BFR31.PRM         Date: Oct 1992
*
.MODEL  BFR31   NJF
+             VTO = -1.0686E+000
+            BETA = 1.73071E-003
+          LAMBDA = 2.29157E-002
+              RD = 9.05115E+000
+              RS = 9.05115E+000
+              IS = 1.70538E-016
+            CGS  = 2.20000E-012
+            CGD  = 2.20000E-012
+              PB = 9.78591E-001
+              FC = 5.00000E-001
*Parameter with default value: FC

*PHILIPS SEMICONDUCTORS        Version 1.0
*Filename: BF556A.PRM       Date: Jan 1993
*
.MODEL  BF556A   NJF
+             VTO = -2.1333E+000
+            BETA = 1.06491E-003
+          LAMBDA = 1.68673E-002
+              RD = 1.41231E+001
+              RS = 1.41231E+001
+              IS = 3.50865E-016
+            CGS  = 2.10000E-012
+            CGD  = 2.30000E-012
+              PB = 7.73895E-001
+              FC = 5.00000E-001
*Parameter with default value: FC

* BF861A NJF model
* created using Parts release 6.2 on 07/20/95 at 14:54
* Parts is a MicroSim product.
.MODEL BF861A NJF
+ VTO=-.5111
+ BETA=15.19E-3
+ LAMBDA=35.93E-3
+ IS=410.2E-18
+ ALPHA=1.000E-6
+ VK=1
+ RD=4.164
+ RS=4.164
+ CGD=6.299E-12
+ CGS=6.299E-12
+ PB=.6917
+ KF=21.54E-18
+ AF=.7958
+ BETATCE=-.5
+ VTOTC=-2.500E-3
*


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,922件の閲覧回数
LPP
NXP Employee
NXP Employee

I found these definitions:

*PHILIPS SEMICONDUCTORS        Version: 1.0
*Filename: BFR31.PRM         Date: Oct 1992
*
.MODEL  BFR31   NJF
+             VTO = -1.0686E+000
+            BETA = 1.73071E-003
+          LAMBDA = 2.29157E-002
+              RD = 9.05115E+000
+              RS = 9.05115E+000
+              IS = 1.70538E-016
+            CGS  = 2.20000E-012
+            CGD  = 2.20000E-012
+              PB = 9.78591E-001
+              FC = 5.00000E-001
*Parameter with default value: FC

*PHILIPS SEMICONDUCTORS        Version 1.0
*Filename: BF556A.PRM       Date: Jan 1993
*
.MODEL  BF556A   NJF
+             VTO = -2.1333E+000
+            BETA = 1.06491E-003
+          LAMBDA = 1.68673E-002
+              RD = 1.41231E+001
+              RS = 1.41231E+001
+              IS = 3.50865E-016
+            CGS  = 2.10000E-012
+            CGD  = 2.30000E-012
+              PB = 7.73895E-001
+              FC = 5.00000E-001
*Parameter with default value: FC

* BF861A NJF model
* created using Parts release 6.2 on 07/20/95 at 14:54
* Parts is a MicroSim product.
.MODEL BF861A NJF
+ VTO=-.5111
+ BETA=15.19E-3
+ LAMBDA=35.93E-3
+ IS=410.2E-18
+ ALPHA=1.000E-6
+ VK=1
+ RD=4.164
+ RS=4.164
+ CGD=6.299E-12
+ CGS=6.299E-12
+ PB=.6917
+ KF=21.54E-18
+ AF=.7958
+ BETATCE=-.5
+ VTOTC=-2.500E-3
*


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,921件の閲覧回数
ucetnahranie
Contributor I

Thank you very much for your response Pavel. Have a nice day!

0 件の賞賛