I'm working on a crystal oscillator using SA602 mixer. In the datasheet Fig.6a How do I determine the values of the capacitors C1 and C2? Assuming that I want to oscillate at the fundamental freq. of the crystal.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm working on a crystal oscillator using SA602 mixer. In the datasheet Fig.6a How do I determine the values of the capacitors C1 and C2? Assuming that I want to oscillate at the fundamental freq. of the crystal.

ソリューションへジャンプ
997件の閲覧回数
rsjaw14
Contributor I
ラベル(1)
  • RF

0 件の賞賛
返信
1 解決策
837件の閲覧回数
LPP
NXP Employee
NXP Employee

L1,C3 elements are not required for fundamental frequency oscillator.

C1=10pF typical
C2[pF]~ 1000/F[MHz]


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
838件の閲覧回数
LPP
NXP Employee
NXP Employee

L1,C3 elements are not required for fundamental frequency oscillator.

C1=10pF typical
C2[pF]~ 1000/F[MHz]


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信