How to use SJA1110 to drive SGMII external phy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use SJA1110 to drive SGMII external phy

Jump to solution
601 Views
Ethan_L
Contributor III

Hi Community,

I want to use SJA1110 to drive SGMII external phy and I need to write to the phy register via MDIO first.

So I think I need to set "SJA1110 SGMII" and "External", but I cannot set both at the same time in S32DS.

Is this correct, or how should I config it?

Ethan_L_0-1679991271085.png

Thanks,

Ethan.

0 Kudos
Reply
1 Solution
579 Views
kaden
NXP Employee
NXP Employee

Hi @Ethan_L 

PHY type "SJA1110 SGMII" only refers to the internal SGMII IP inside the respective SJA1110 ports. Thus, in your case, you probably have to choose PHY type "Generic" and PHY location "External". This way you can have access to the PHY via the SMI interface and configure the PHY accordingly. 

 

Best regards

Kevin 

View solution in original post

0 Kudos
Reply
1 Reply
580 Views
kaden
NXP Employee
NXP Employee

Hi @Ethan_L 

PHY type "SJA1110 SGMII" only refers to the internal SGMII IP inside the respective SJA1110 ports. Thus, in your case, you probably have to choose PHY type "Generic" and PHY location "External". This way you can have access to the PHY via the SMI interface and configure the PHY accordingly. 

 

Best regards

Kevin 

0 Kudos
Reply