How to "disconnect" one port of the PCA9698?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to "disconnect" one port of the PCA9698?

1,005件の閲覧回数
michel_coriat
Contributor I


Hello,

For some reasons, one port of the PCA9698 is connected to the analog output of a sensor. I know, this is not the optimal situation.

Is this situaton disturbing for the PCA9698? If yes, how can I programmatically (with internal register of the PCA9698) "disconnect" this port to not disturb the PCA9698? declare it as output ports with open-drain? any alternative solution?


thank you for your responses

regards,
Michel

0 件の賞賛
5 返答(返信)

885件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

OK,You can send the pin of PCA9698 which connected with sensor as input configuration.

0 件の賞賛

885件の閲覧回数
michel_coriat
Contributor I

The sensor use an unique bidirectional pin. Depending on the sensor configuration, that pin can either: output analog signal, output or input binary signal (HIGH or LOW) or input PWM signal. 

So when the sensor is configured as analog output, do you think it would disturb the PCA9698? How to avoid it?

0 件の賞賛

885件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Do you want to take the sensor analog output as input of PCA9698?

0 件の賞賛

885件の閲覧回数
michel_coriat
Contributor I

yes, but the sensor analog output is also connected to the ADC pin of the microcontroller to do ADC conversion.

0 件の賞賛

885件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

What's your purpose to connect the IO pin to output of sensor?

0 件の賞賛