How to "disconnect" one port of the PCA9698?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to "disconnect" one port of the PCA9698?

998 Views
michel_coriat
Contributor I


Hello,

For some reasons, one port of the PCA9698 is connected to the analog output of a sensor. I know, this is not the optimal situation.

Is this situaton disturbing for the PCA9698? If yes, how can I programmatically (with internal register of the PCA9698) "disconnect" this port to not disturb the PCA9698? declare it as output ports with open-drain? any alternative solution?


thank you for your responses

regards,
Michel

0 Kudos
5 Replies

878 Views
guoweisun
NXP TechSupport
NXP TechSupport

OK,You can send the pin of PCA9698 which connected with sensor as input configuration.

0 Kudos

878 Views
michel_coriat
Contributor I

The sensor use an unique bidirectional pin. Depending on the sensor configuration, that pin can either: output analog signal, output or input binary signal (HIGH or LOW) or input PWM signal. 

So when the sensor is configured as analog output, do you think it would disturb the PCA9698? How to avoid it?

0 Kudos

878 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you want to take the sensor analog output as input of PCA9698?

0 Kudos

878 Views
michel_coriat
Contributor I

yes, but the sensor analog output is also connected to the ADC pin of the microcontroller to do ADC conversion.

0 Kudos

878 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

What's your purpose to connect the IO pin to output of sensor?

0 Kudos