How to output Information in Serial Port about OM40007

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to output Information in Serial Port about OM40007

789 Views
afzhang
Contributor I

Hi,man.

I have OM40007:LPC54018 IoT Module for the LPC540XX family of MCUs, but i do not know how to debug.

How to output Information in Serial Port.

0 Kudos
Reply
2 Replies

744 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 爱飞 张,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It should work with the baseboard (OM4006) which provides the onboard debugger and some several peripherals.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

744 Views
afzhang
Contributor I

Hi jeremyzhou:

Thanks!

B/R

Aifei Zhang

发件人: jeremyzhou

发送时间: 2019年7月9日 10:39

收件人: Aifei Zhang

主题: Re: - Re: How to output Information in Serial Port about OM40007

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How to output Information in Serial Port about OM40007

reply from jeremyzhou <https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in Other NXP Solutions - View the full discussion <https://community.nxp.com/message/1175172?commentID=1175172&et=watches.email.thread#comment-1175172>

0 Kudos
Reply