How to download the external flash of S32R294 from S32 Design Studio for Power Architecure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to download the external flash of S32R294 from S32 Design Studio for Power Architecure

跳至解决方案
526 次查看
HyunungPark
Contributor III

Currently, I am using S32R294.

and I want to download the external flash of S32R294 from S32 Design Studio for Power Architecure.

As I know, the code of external flash is copied to SRAM when boot because there is no internal flash in s32r294.

Could you please let me know and the document for the above two item?

BRs.

Hyunung Park

0 项奖励
1 解答
508 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.

So you only then need to read RAM in your debug session.

There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.

Best regards,

Peter

在原帖中查看解决方案

0 项奖励
1 回复
509 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.

So you only then need to read RAM in your debug session.

There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.

Best regards,

Peter

0 项奖励