How to download the external flash of S32R294 from S32 Design Studio for Power Architecure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download the external flash of S32R294 from S32 Design Studio for Power Architecure

ソリューションへジャンプ
592件の閲覧回数
HyunungPark
Contributor III

Currently, I am using S32R294.

and I want to download the external flash of S32R294 from S32 Design Studio for Power Architecure.

As I know, the code of external flash is copied to SRAM when boot because there is no internal flash in s32r294.

Could you please let me know and the document for the above two item?

BRs.

Hyunung Park

0 件の賞賛
返信
1 解決策
574件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.

So you only then need to read RAM in your debug session.

There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.

Best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
575件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.

So you only then need to read RAM in your debug session.

There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.

Best regards,

Peter

0 件の賞賛
返信