How to download the external flash of S32R294 from S32 Design Studio for Power Architecure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download the external flash of S32R294 from S32 Design Studio for Power Architecure

Jump to solution
591 Views
HyunungPark
Contributor III

Currently, I am using S32R294.

and I want to download the external flash of S32R294 from S32 Design Studio for Power Architecure.

As I know, the code of external flash is copied to SRAM when boot because there is no internal flash in s32r294.

Could you please let me know and the document for the above two item?

BRs.

Hyunung Park

0 Kudos
Reply
1 Solution
573 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.

So you only then need to read RAM in your debug session.

There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.

Best regards,

Peter

View solution in original post

0 Kudos
Reply
1 Reply
574 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.

So you only then need to read RAM in your debug session.

There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.

Best regards,

Peter

0 Kudos
Reply