I use "fsl-auto-rsdk-bsp-v33.0.tar.gz" to build fsl-image-auto.
How should I modify the device tree to support nvme?
It' my device tree
serdes0: serdes@40480000 {
#phy-cells = <3>;
compatible = "nxp,s32cc-serdes";
clocks = <&clks S32GEN1_SCMI_CLK_SERDES_AXI>,
<&clks S32GEN1_SCMI_CLK_SERDES_AUX>,
<&clks S32GEN1_SCMI_CLK_SERDES_APB>,
<&clks S32GEN1_SCMI_CLK_SERDES_REF>;
clock-names = "axi", "aux", "apb", "ref";
resets = <&reset S32GEN1_SCMI_RST_SERDES0>,
<&reset S32GEN1_SCMI_RST_PCIE0>;
reset-names = "serdes", "pcie";
fsl,sys-mode = <PCIE_GEN3X2_MODE>;
reg = <0x0 0x40480000 0x0 0x108>,
<0x0 0x40483008 0x0 0x10>,
<0x0 0x40482000 0x0 0x800>,
<0x0 0x40482800 0x0 0x800>;
reg-names = "ss_pcie", "pcie_phy", "xpcs0", "xpcs1";
status = "okay";
};
but.
[ 1.548300] phy-s32gen1-serdes 40480000.serdes: Using mode 0 for SerDes subsystem
[ 1.548970] phy-s32gen1-serdes 44180000.serdes: Using mode 0 for SerDes subsystem
[ 1.549965] phy_mode = 0 40400000.pcie: Configured as RootComplex
[ 1.549970] sctrl->ext_clk=1
[ 1.549973] start!
[ 1.554963] end!
[ 1.554971] phy-s32gen1-serdes 40480000.serdes: Failed to lock PCIE phy
[ 1.554980] phy phy-40480000.serdes.0: phy poweron failed --> -110
Hello,
The BSP 33 should support the NVMe via PCIe by default. When booting, U-Boot should detect the device. Please refer to the attached image. In Linux, the device is detected under /dev/nvme0 and /dev/nvme0n1. You can create a partition in /dev/nvme0n1 with fdisk and format it via mkfs.ext3.
Hi
It seems to me a clock problem. Can you try the below command in Uboot? and check the clock frequencies? On my side I get the next output:
=> verifclk CMU | Monitored | Reference | Expected | Verified
ID CLOCK CLOCK RANGE (MHZ) RANGE (MHZ)
0 | FXOSC | FIRC | 40.000 | 39.062 |
1 | FIRC | FXOSC | 48.000 | 48.146 |
2 | SIRC | FXOSC | 0.032 | 0.031 |
3 | FTM_0_REF | FXOSC | 40.000 | 39.976 |
4 | FTM_1_REF | FXOSC | 40.000 | 39.976 |
5 | XBAR_DIV3 | FIRC | 133.333 | 125.000 |
6 | XBAR_M7_0 | FIRC | 400.000 | 375.000 |
7 | XBAR_DIV3 | FXOSC | 133.333 | 132.812 |
8 | XBAR_M7_1 | FIRC | 400.000 | 375.000 |
9 | XBAR_M7_2 | FIRC | 400.000 | 375.000 |
10 | PER | FIRC | 80.000 | 78.125 |
11 | SERDES_REF | FXOSC | 100.000 - 125.000 | 99.609 |
12 | FLEXRAY_PE | FXOSC | 40.000 | 0.000 - 0.015 |
13 | CAN_PE | FXOSC | 80.000 | 80.078 |
14 | GMAC_0_TX | FXOSC | 125.000 | 125.000 |
15 | GMAC_TS | FXOSC | 200.000 | 0.000 - 0.015 |
16 | LIN | FXOSC | 125.000 | 62.500 |
17 | QSPI_1X | FXOSC | 133.333 | 132.812 |
18 | SDHC | FXOSC | 400.000 | 398.437 |
20 | DDR | FIRC | 800.000 | 750.000 |
21 | GMAC_0_RX | FXOSC | 2.500 - 125.000 | 24.902 |
22 | SPI | FXOSC | 100.000 | 99.609 |
27 | A53_CORE | FXOSC | 800.000 | 796.875 |
28 | A53_CORE | FIRC | 800.000 | 750.000 |
38 | ACCEL3 | FXOSC | 600.000 | 601.562 |
39 | ACCEL4_0 | FXOSC | 400.000 | 398.437 |
40 | ACCEL4_0 | FXOSC | 400.000 | 398.437 |
46 | GMAC_1_TX | FXOSC | 125.000 | 0.000 - 0.015 |
51 | GMAC_1_RX | FXOSC | 125.000 | 47.851 |
52 | MIPICSI2_0 | FXOSC | 400.000 | 398.437 |
53 | MIPICSI2_0 | FXOSC | 400.000 | 398.437 |
54 | SERDES_REF | FXOSC | 125.000 | 99.609 |
After this, you can try to use the internal clock instead: The customer has to modify the next environment variable in Uboot:
=> print hwconfig
hwconfig=pcie0:mode=rc,clock=ext;pcie1:mode=ep,clock=int
=> edit hwconfig
edit: pcie0:mode=rc,clock=int;pcie1:mode=ep,clock=int
=> saveenv
Saving Environment to MMC... Writing to MMC(0)... OK
Then reset the board and see if the MPLLs is still unlocked.
Please share the results.
Hi
Our board hardware has a power supply problem,Now it can detect nvme。
in addition,we find write speed is too slow in cache mode(170MB/s)。Direct mode seems to be normal(852MB/s).
root@s32r45evb:/mnt/nvme# dd if=/dev/zero of=test bs=8M count=256
256+0 records in
256+0 records out
2147483648 bytes (2.1 GB, 2.0 GiB) copied, 12.5997 s, 170 MB/s
root@s32r45evb:/mnt/nvme# dd if=/dev/zero of=test bs=8M count=256 oflag=direct
256+0 records in
256+0 records out
2147483648 bytes (2.1 GB, 2.0 GiB) copied, 2.52067 s, 852 MB/s
We wrote a test program,The average write speed is around 250MB/s,.here's still a gap in the write speed that we want.
Why is cache mode lower than direct mode?
Can it be optimized?
Thanks