Hi,everybody,i'm using DSC MC56F8366 and developing Bootloader for it.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi,everybody,i'm using DSC MC56F8366 and developing Bootloader for it.

406件の閲覧回数
wzqwzq
Contributor I

I download my applitions with SCI.But i only can download with 9600 bps.When I use 19200,56000,115200.....,MCU always return an error.Can you help me?

0 件の賞賛
2 返答(返信)

313件の閲覧回数
Ben
Senior Contributor I

Hi XianJun, I have an active developments with the NC56F8367 and the 56F8257. I did not activate the bootloader yet, but I don't understand:

Did you have a  problem with freescale bootloader application? why did you have to develop your own SW?

Sorry that I can't answer your question yet, but I'll be glad to get any tip for me for the bootloader  issue, as I'll have to add bootloader.

Thanks

Benny

0 件の賞賛

313件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

sorry for the delay, I see your question just now. I do not know if you have solved your problem or not yet.

If you want to use the other baud rate, the baud rate in the bootloader code and the HyperTerminal setting should matches, I suppose you download code via Hyperterminal tools.

BR

XiangJun Rong