Hi, Please provide source and load impedance details at 108Mhz to 138Mhz frequency range for MRF6V2150NR1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, Please provide source and load impedance details at 108Mhz to 138Mhz frequency range for MRF6V2150NR1

658件の閲覧回数
ajivs
Contributor I

Hi, Please provide source and load impedance details at  108Mhz  to 138Mhz frequency range for MRF6V2150NR1

0 件の賞賛
返信
2 返答(返信)

563件の閲覧回数
LPP
NXP Employee
NXP Employee

We have no measured data at these frequencies.

Input and load impedances simulated with MRF6V2150NR1 ADS model.

Optimized for best PAE or P1dB power at 1dB output compression.

maximum Power
    Input        Load
108    3.49-j11.05    3.65+j2.32
138    2.67-j9.33    3.65+j2.32

maximum PAE
    Input        Load
108    3.41-j10.4    4.67+j4.82
138    2.52-j9.02    3.32+j3.89

Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

563件の閲覧回数
ajivs
Contributor I

Hi

Thanks for the feedback. However I am unable to download ADS Model for this part. "Page Not Found" window appears after clicking download button.

Please share this data.

Regards

Aji

0 件の賞賛
返信