Freescale Beestack Over The Air Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale Beestack Over The Air Update

Jump to solution
951 Views
Loris83
Contributor II

I'm using Freescale Test Tool 11.3.0 with an Evaluation kit mc13224.

I'm using Beestack codebase.

Using Beekit I have enabled the OTA server (on the coordinator) and the OTA client (on the other device, router)

I've tried to use the "OTA Update" supplied by Test Tool, with a *.bin file generated by IAR 6.10.

 

The update starts, the server send the update,

but I receive an Abort message, and the client resets itself.

(I can see these steps through the "Message Log" displayed in the OTA Update window)

 

Is "OTA Update" working with Beestack codebase?

 

Someone could help me?

0 Kudos
1 Solution
584 Views
Loris83
Contributor II

Hi martinhp,

 

First of all: thank you for your answer.

 

I'm using codebase 3.0.11, with IAR 6.10, and Beekit.

 

The OTA Update works, I was using a wrong configuration, for the OTA client. The main problem is the lack of a manual for this interesting functionality.

 

Do you know a good documentation for this functionality?

 

 

 

View solution in original post

0 Kudos
2 Replies
584 Views
martinhp
Contributor I

 

What code code base are you using?  3.0.11?

 

The latest codebase is for the IAR 5.50 not for the 6.10.. try with this. may be this is causing the problem.

 

Regards,

Martin

0 Kudos
585 Views
Loris83
Contributor II

Hi martinhp,

 

First of all: thank you for your answer.

 

I'm using codebase 3.0.11, with IAR 6.10, and Beekit.

 

The OTA Update works, I was using a wrong configuration, for the OTA client. The main problem is the lack of a manual for this interesting functionality.

 

Do you know a good documentation for this functionality?

 

 

 

0 Kudos