Fast Ethernet Media Converter 10BASE-T1 Compatibilty

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fast Ethernet Media Converter 10BASE-T1 Compatibilty

643 次查看
Marco846
Contributor I

Hello,

is your 2-wire Ethernet (100BASE-T1) to Fast Ethernet (100BASE-TX) Media Converter

RDDRONE-T1ADAP

also compatible with the slower 2-wire Ethernet 10BASE-T1S or 10BASE-T1L standard?

Best regards

0 项奖励
1 回复

637 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

Yes, RDDRONE-T1ADAP is based on the TJA1101B Ethernet PHY, and if it is configured properly, this device is also compatible with 10 Mbit/s speed, to do this you need to configure the Speed Select bits to ‘00’ (SPEED_SELECT (MSB) = 0 and SPEED_SELECT (LSB) = 0).

Regards,

Jose

 

0 项奖励