Factors causing / HRST of MPC8270

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Factors causing / HRST of MPC8270

591 Views
HiroyukiO
Contributor I
We are investigating defects on the board. Even though / PORST is always H input to MPC8270 on the board, pulses are periodically output from / HRST and / SRST and reset is applied. What are the possible causes? ・ The pulse width of / HRST is 16us, and / SRST is almost the same. ・ The pulse interval of / HRST is more than 10 seconds, and / SRST is almost the same. ・ The power supply and clock are normal. ・ There is one CPU on the board. ・ Softwarewatchdog is invalid ・ Checkstop has not occurred Thank you
0 Kudos
3 Replies

584 Views
Bulat
NXP Employee
NXP Employee

Try to read Reset Status Register (RSR) after reset, it provides information about reason of reset.

Regards,

Bulat

 

0 Kudos

573 Views
Ohata
Contributor I

I checked the RSR using a debugger, but couldn't find any particular cause. I suspect Check Stop, but the output signal / CK_STP_OUT was not in Check Stop Mode either.

Thank you,

hiroyukiO

 

0 Kudos

559 Views
Bulat
NXP Employee
NXP Employee

All possible reasons of HRESET assertion are listed in section 5.1.1 of the manual. Checkstop reset can happen only if you set RMR[CSRE] bit.

Regards,

Bulat

 

0 Kudos