hello
I have the same question as below.
I too would like an answer.
https://community.nxp.com/t5/Power-Management/FS26-sbc-watchdog-notification/m-p/1803185
Hi, I am using Sbc_fs26_example project. I realized in the main of this project we do not reload the sbc wdg. I saw SbcWatchdogNotification and i think if i use this i will have to reload the watchdog periodically. But when i added i saw that inside of the function was empty. Is there any example about this which i can use?
HI Joao,
the watchdog notification can be call only when the wdg configuration changes
where the Watchdog refresh notification is called after each refresh, to optionally evaluate the flags
best regards
Jochen
Hello Junyeong ,
Are you using the new release of the FS26 driver?
The release is available from our NXP FlexNet Operations:
BRs, Tomas
Hello @TomasVaverka ,
I do have those drivers installed, but the Wdg driver is for use in a AUTOSAR context, which i'm not yet interested in. Thus, is there any documentation on how to implement the SBC Watchdog Notification?
I have created a callback function as "void WatchdogCallback (void)" but, when compiling the program, it gives an error saying i'm missing some arguments, more specifically, "const uint8 WindowPeriod, const uint8 WindowDc". But this gets me confused, because the description of the SbcWatchdogNotification is to call the Sbc_fs26_WdgRefresh() API function, which doesn't receive any arguments. So, how should i implement this?
Thanks in advance,
JRodrigues