FRDM-KEAZ64 SDK download fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KEAZ64 SDK download fail

773件の閲覧回数
547416104
Contributor III

Hello everyone,

I can down load the FRDM-KEAZ64 SDK from NXP web, I do not know whether it has SDK or not, if you have it, could you help to send it to me, thanks.

I used develop IDE is S32DS.

0 件の賞賛
3 返答(返信)

766件の閲覧回数
nxf45548
NXP Employee
NXP Employee

Thank you for contacting NXP Technical support. 
To provide you with better support, can you please be more specific with the error you receive when you try to download the software? 
Also, can you please share the link that you are using to download it? 
Are  you download it from the following link: 
https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/kea-automotive-mcu...


0 件の賞賛

622件の閲覧回数
547416104
Contributor III

I just use IDE(S32DS) to creat FRDM_SKEAZ64 project, there's no correspond KEAZ64 SDK for selected. whether can select KEAZ128 SDK for SKEAZ64?

0 件の賞賛

765件の閲覧回数
nxf45548
NXP Employee
NXP Employee

@547416104 

On the other hand, I suggest you try to download the software using an incognito/ private window win Chrome/ Firefox as sometimes cookies block the option to log in properly. 

0 件の賞賛