Extra Pin control with SPIGEN 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Extra Pin control with SPIGEN 7

461 Views
Fast
Contributor IV

What might prevent SPIGEN 7 using FRDM-KL25Z  to control FRDMPKPT2000EVM with the Extra Pins, listed in generic commands? Is there no read back to signal fault?

Labels (1)
0 Kudos
Reply
2 Replies

442 Views
Fast
Contributor IV

Yes thank you XiangJun Rong, seems that the DRVEN is not controlled, I assume this is a HW issue with my FRDM-KL25Z. I believe the code is loaded and runs to some extent as I cab read the Bat voltage. Is there no read back to signal fault? Will re post on the auto community.

 

0 Kudos
Reply

447 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls download the KTPT2000FRDM3CUG.pdf from the link.

https://www.nxp.com.cn/docs/en/user-guide/KTPT2000FRDM3CUG.pdf

The above doc lists the signal connection between FRDM-KL25Z and FRDMPKPT2000EVM.

The FRDMPKPT2000EVM is Auto board, you'd better to post question on the auto community.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply