Does the BGA2866 invert an input pulse?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the BGA2866 invert an input pulse?

664件の閲覧回数
johneberly
Contributor I

I'm having trouble getting this question answered. I could purchase a Demoboard for the BGA2866, but the NXP website returns a demoboard for a BGU6010,2,etc. when I search and that is the wrong package.

タグ(1)
0 件の賞賛
返信
1 返信

601件の閲覧回数
LPP
NXP Employee
NXP Employee

BGA2866 doesn't invert the input signal.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信