Does NXP have beamformers that can support bands from 33GhZ to 37GhZ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP have beamformers that can support bands from 33GhZ to 37GhZ?

Jump to solution
1,129 Views
shai_b
Senior Contributor II

Hello Team,

Could you please advise back if NXP has beamformers devices that can support bands from 33GhZ to 37GhZ?

Thanks in advance.

Kind Regards,

Shai

0 Kudos
Reply
1 Solution
1,114 Views
LPP
NXP Employee
NXP Employee

We have no devices that can support bands from 33GHz to 37GHz. NXP offers MMW9004KC for 26GHz (n258 band), MMW9002KC for 28GHz (n257 band), MMW9003KC for 39GHz (n260 band). New devices are forthcoming but for the same frequency bands.

Best Regards,

Pavel

NXP CAS

 

View solution in original post

0 Kudos
Reply
3 Replies
1,115 Views
LPP
NXP Employee
NXP Employee

We have no devices that can support bands from 33GHz to 37GHz. NXP offers MMW9004KC for 26GHz (n258 band), MMW9002KC for 28GHz (n257 band), MMW9003KC for 39GHz (n260 band). New devices are forthcoming but for the same frequency bands.

Best Regards,

Pavel

NXP CAS

 

0 Kudos
Reply
1,093 Views
shai_b
Senior Contributor II

@LPP Dear Pavel,

Could you please share the datasheet of MMW9003KC, this part could be very interesting.

Thanks in advance.

Kind regards,

Shai 

Tags (1)
0 Kudos
Reply
1,111 Views
shai_b
Senior Contributor II

@LPP Hi Pavel,

Thank you so much for your inputs.

KR,

Shai

0 Kudos
Reply