Dealing with Thermal Pad of PCAL6524HEAZ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dealing with Thermal Pad of PCAL6524HEAZ

ソリューションへジャンプ
706件の閲覧回数
Edgard
Contributor III

Dear an Engineer in NXP

I have one question about the Thermal Pad of PCAL6524HEAZ.
I checked the comment that the Thermal Pad is not connected to internal chip directly.

Is it NOT necessary to connect to GND pattern on PCB with the Thermal Pad?

Thanks in advance
Edgard

0 件の賞賛
返信
1 解決策
680件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eduard,

you are correct. The thermal pad underneath the PCAL6524HEAZ is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

With Best Regards,

Jozef

元の投稿で解決策を見る

2 返答(返信)
681件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eduard,

you are correct. The thermal pad underneath the PCAL6524HEAZ is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

With Best Regards,

Jozef

676件の閲覧回数
Edgard
Contributor III
Dear Jozef

thanks for your quick response.
I may connect the Thermal PAD to GND.

Kindest Regards
Edgard