Dealing with Thermal Pad of PCAL6524HEAZ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dealing with Thermal Pad of PCAL6524HEAZ

Jump to solution
505 Views
Edgard
Contributor III

Dear an Engineer in NXP

I have one question about the Thermal Pad of PCAL6524HEAZ.
I checked the comment that the Thermal Pad is not connected to internal chip directly.

Is it NOT necessary to connect to GND pattern on PCB with the Thermal Pad?

Thanks in advance
Edgard

0 Kudos
Reply
1 Solution
479 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eduard,

you are correct. The thermal pad underneath the PCAL6524HEAZ is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

With Best Regards,

Jozef

View solution in original post

2 Replies
480 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eduard,

you are correct. The thermal pad underneath the PCAL6524HEAZ is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

With Best Regards,

Jozef

475 Views
Edgard
Contributor III
Dear Jozef

thanks for your quick response.
I may connect the Thermal PAD to GND.

Kindest Regards
Edgard