Data streaming issue and Frame Rate Problem in IMX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Data streaming issue and Frame Rate Problem in IMX8

Jump to solution
1,937 Views
shrithi
Contributor I
I have developed the custom driver for MIPI CSI2 FPGA IP support. MIPI CSI2 FPGA IP send the data to MIPI RX.
I have configured 4 data lanes for mipi and below configuration defined in device-tree
 
/* FPGA MIPI configuration */
&mipi_csi_0 { /* MIPI_CSI0: FPGA L MIPI TX */
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
 
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&fpga_L_mipi_ep>;
data-lanes = <1 2 3 4>;
bus-type = <4>;
};
};
};
 
&i2c_mipi_csi0 { /* MIPI_CSI0: FPGA L TX */
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c_mipi_csi0>;
clock-frequency = <400000>;
status = "okay";
 
fpga_L_mipi: fpga_L_mipi@3c {
compatible = "mipi,custom_mipi";
reg = <0x3c>;
mipi_csi;
status = "okay";
port {
fpga_L_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
clocks-lanes = <0>;
};
};
};
};
 
When I enabled 4 lanes it will stuck during streaming
root@host:~# gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=1 ! video/x-raw,format=RGB,width=1920,height=1080,framerate=10/1 ! filesink location=test2.raw
[  424.947801] bypass csc
[  424.950169] input fmt RGB4
[  424.952909] output fmt RGB3
 
Later I enabled 2 lines in device-tree. With 2lanes, some times we are able to get the data, but this is not stable. I used the FPGA MIPI TX IP which supports RGB24 format. we configured the FPGA MIPI TX at 125MHZ mipi clock for 1980x1080@30fps but we received less than 10fps in imx8.
 
root@host:~# v4l2-ctl -d /dev/video0 --set-fmt-video=width=1920,height=1080,pixelformat=RGB3 --stream-mmap
[ 140.157118] bypass csc
[ 140.159501] input fmt RGB4
[ 140.162205] output fmt RGB3
<<<<<<<<<< 8.73 fps
<<<<<<<< 7.53 fps
<<<<<< 7.53 fps
<<<< 6.66 fps
 
Can you please tell us what I am missing? How to configure clock in imx side?
Please help me to solve this problem.
 
Thank you.
0 Kudos
Reply
1 Solution
1,486 Views
joanxie
NXP TechSupport
NXP TechSupport

you don't need change escape clock, as I mentioned before, you need check your FPGA side clock, if could, pls measure the mipi  clock  by oscilloscope to check if correct or not I also attached the mipi guide to reference

View solution in original post

0 Kudos
Reply
20 Replies
400 Views
zhanghaijian
Contributor II

hey ,shrithi!

 I have encountered the same problem with you,have you solved it right now?if you can,could you share your fpga mipi driver code,very appreciate that。

0 Kudos
Reply
1,877 Views
shrithi
Contributor I

I seen below hs setting value in drivers/staging/media/imx/imx8-mipi-csi2.c driver. How hs_setting value calculated based on width, height and framerate? Example: width=3056 height=3056 framerate=10 , in this case what is the hs_setting value?

static struct mxc_hs_info hs_setting[] = {
{2592, 1944, 30, 0x0B},
{2592, 1944, 15, 0x10},

{1920, 1080, 30, 0x0B},
{1920, 1080, 15, 0x10},
{1920, 1080, 25, 0x0C},

{1280, 720, 30, 0x11},
{1280, 720, 15, 0x16},

{1024, 768, 30, 0x11},
{1024, 768, 15, 0x23},

{720, 576, 30, 0x1E},
{720, 576, 15, 0x23},

{720, 480, 30, 0x1E},
{720, 480, 15, 0x23},

{640, 480, 30, 0x1E},
{640, 480, 15, 0x23},

{320, 240, 30, 0x1E},
{320, 240, 15, 0x23},

{176, 144, 30, 0x1E},
{176, 144, 15, 0x23},
};

0 Kudos
Reply
1,914 Views
shrithi
Contributor I
yes. I am using i.MX8 QM processor.
 
Can you explain about clock configuration?  How to calculate clk_core and clk_esc?    
clock-names = "clk_core", "clk_esc", "clk_pxl";
When I set clock configuration as below I am getting data with 4 data lanes and fps it showing 180fps.
assigned-clock-rates = <266000000>, <333000000>, <66000000>
 
Device-tree mentioned as below
/* FPGA MIPI configuration */
&mipi_csi_0 { /* MIPI_CSI0: FPGA L MIPI TX */
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
 
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&fpga_L_mipi_ep>;
data-lanes = <1 2 3 4>;
bus-type = <4>;
};
};
};
 
&i2c_mipi_csi0 { /* MIPI_CSI0: FPGA L TX */
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c_mipi_csi0>;
clock-frequency = <400000>;
status = "okay";
 
fpga_L_mipi: fpga_L_mipi@3c {
compatible = "mipi,custom_mipi";
reg = <0x3c>;
mipi_csi;
status = "okay";
port {
fpga_L_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
clocks-lanes = <0>;
};
};
};
};
0 Kudos
Reply
1,901 Views
joanxie
NXP TechSupport
NXP TechSupport

why I ask for other dts files, I need to know how you set clock for mipi csi, I don't know what you change, but for imx8qm, I checked current bsp already supports 4 data lane,

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8qm-mek.dts

&mipi_csi_0 {
#address-cells = <1>;
#size-cells = <0>;
virtual-channel;
status = "okay";

/* Camera 0 MIPI CSI-2 (CSIS0) */
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&max9286_0_ep>;
data-lanes = <1 2 3 4>;
};
};
};

for imx8qm mipi csi clock,  only set core clock and esc clock, since current bsp can support 4 data lane, you can refer to the setting as below

mipi_csi_0: csi@58227000 {
compatible = "fsl,mxc-mipi-csi2";
reg = <0x58227000 0x1000>,
<0x58221000 0x1000>;
clocks = <&csi0_core_lpcg 0>,
<&csi0_esc_lpcg 0>,
<&csi0_pxl_lpcg 0>;
clock-names = "clk_core", "clk_esc", "clk_pxl";
assigned-clocks = <&csi0_core_lpcg 0>,
<&csi0_esc_lpcg 0>;
assigned-clock-rates = <360000000>, <72000000>;
power-domains = <&pd IMX_SC_R_CSI_0>, <&pd IMX_SC_R_ISI_CH0>;
power-domain-names = "pd_csi", "pd_isi_ch0";
status = "disabled";
};

0 Kudos
Reply
1,891 Views
shrithi
Contributor I

With this assigned-clock-rates = <360000000>, <72000000>; I am not able to stream the data. So I changed to  assigned-clock-rates = <200000000>, <333000000>; Is this proper?

Based on documents I assigned core clock as 200MHz. But I am not sure about esc clock.

Screenshot from 2024-03-22 09-52-13.png

0 Kudos
Reply
1,801 Views
joanxie
NXP TechSupport
NXP TechSupport

escape clock is for low power, normally customer doesn't need to change it, do you mean you can boot up 2 data lane with assigned-clock-rates = <360000000>, <72000000>; but failed with 4 data lane, then you change it to <200000000>, <333000000>; the 4 data lane setting works, right? you don't change anything else?

0 Kudos
Reply
1,797 Views
shrithi
Contributor I

We are able to get the data using 2 lanes with <360000000>, <72000000> (inconsistent). With <200000000>, <333000000> setting I am able to stream the data with 4 lanes. No other software changes done, TX mipi pixel clock changed to 74.25MHz, output clock is 222.75MHz and data rate is 445.5. Resolution is 1920*1080@30fps. 

0 Kudos
Reply
1,785 Views
joanxie
NXP TechSupport
NXP TechSupport

current imx8qm bsp already supports 4 data lane, I shared the default code with you before, you should check your own driver, total data rate= pixel clock * Bits-per-pixel, if your pixel clock is 74.25, the data rate shouldn't be 445.5, you need set the correct clock for the MIPI CSI2, then MIPI CSI2 would change it's register to meet your request, so your root cause isn't escape clock in the dts, should check your own driver if your driver set correct clock or not, for example, current bsp supports 4 data lane for max9286, in the max9286 driver, you can find

  /*
   * Pass mipi phy clock rate Mbps
   * fcsi2 = PCLk * WIDTH * CHANNELS / LANES
   * fsci2 = 72MPCLK * 8 bit * 4 channels / 4 lanes
   */
  max9286_data->format.reserved[0] = 72 * 8;

the max9286 uses 288M mipi clock, so pls check your FPGA driver if set this correct or not,

 

0 Kudos
Reply
1,782 Views
shrithi
Contributor I

We used below equations to calculate the clock and data rate
Pixel Clock Hz = HTOT*VTOT*FPS
Bandwidth bps = Pixel Clock * Bits Per Pixel
Data Rate Per Lane bps = Bandwidth / number of data lanes
MIPI D − PHY Clock Rate Hz = Data Rate Per Lane / 2

Pixel Clock = 2200×1125×30 = 74250000 Hz
Bandwidth = 74250000 * 24 = 1782000000 bps
Data Rate Per Lane = 1782000000/4 = 445500000 bps = 445.5 Mbps
MIPI Bit clock = 445500000 / 2 = 222750000 = 222.75 MHz

0 Kudos
Reply
1,765 Views
joanxie
NXP TechSupport
NXP TechSupport

bit_clk = Pixel clock * Bits per pixel / Number of lanes=74.25*24/4=445.5

0 Kudos
Reply
1,763 Views
shrithi
Contributor I

I have gone through the below mentioned document

https://www.nxp.com/docs/en/application-note/AN13573.pdf

equation.png

Can you please reconfirm the calculation once?

0 Kudos
Reply
1,758 Views
joanxie
NXP TechSupport
NXP TechSupport

the equation 16 is for mipi clock, bit clock is another clock, you mentions mipi bit clock, I thought you mean bit clock

0 Kudos
Reply
1,735 Views
shrithi
Contributor I

How 1 pixel per clock and 4 pixel per clock vary in below equation for RGB888 format of data?

Bandwidth bps = Pixel Clock * Bits Per Pixel

Can you explain this? 

0 Kudos
Reply
1,636 Views
joanxie
NXP TechSupport
NXP TechSupport

for example, rgb888 send over 8bits, then needs 3 cycles/pixel, the depth is 24bpp

0 Kudos
Reply
1,620 Views
shrithi
Contributor I

How to calculate esc clock? I am suspecting clock configured by imx8 also. What maximum escape clock supported by imx8?

Currently I assigned 333MHz clock for esc clock.

When I stream data with 30fps, I am getting framerates in the range of 15 to 20.

v4l2-ctl -d /dev/video0 --set-fmt-video=width=1920,height=1080,pixelformat=RGB3 --set-parm=30 --stream-mmap
Frame rate set to 30.000 fps
[ 201.417005] bypass csc
[ 201.419426] input fmt RGB4
[ 201.422509] output fmt RGB3
<<<<<<<<<<<<<<<<<<<<<<< 21.37 fps
<<<<<<<<<<<<<<<<<<<<< 21.29 fps
<<<<<<<<<<<<<<<<< 19.50 fps
<<<<<<<<<<<<<<<<<< 19.60 fps
<<<<<<<<<<<<<<<<<<<<<<<< 20.03 fps
<<<<<<<<<<<<<<<<<< 19.76 fps
<<<<<<<<<<<<<<<<<<<<< 19.72 fps
<<<<<<<<<<<<<<<<< 19.00 fps

The data will not be streamed if I set fps to 15fps. It will hang while streaming the data.
v4l2-ctl -d /dev/video0 --set-fmt-video=width=1920,height=1080,pixelformat=RGB3 --set-parm=15 --stream-mmap
Frame rate set to 15.000 fps
[ 292.933426] bypass csc
[ 292.935842] input fmt RGB4
[ 292.938783] output fmt RGB3

By setting it to 60fps, I will achieve a framerate of 50.
v4l2-ctl -d /dev/video0 --set-fmt-video=width=1920,height=1080,pixelformat=RGB3 --set-parm=60 --stream-mmap
Frame rate set to 60.000 fps
[ 341.047806] bypass csc
[ 341.050182] input fmt RGB4
[ 341.052936] output fmt RGB3
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 50.51 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 50.51 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 50.51 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 50.51 fps

The data on the TX side is set to 1920x1080 at 15 frames per second.
What caused the FPS to change every time? Does the hs_settle value cause the problem? The following values were given as hs_settle values in the driver.

drivers/staging/media/imx/imx8-mipi-csi2.c
static u8 rxhs_settle[3] = {0xD, 0xA, 0x7};
static struct mxc_hs_info hs_setting[] = {
{2592, 1944, 30, 0x0B},
{2592, 1944, 15, 0x10},

{1920, 1080, 30, 0x0B},
{1920, 1080, 15, 0x10},

{1280, 720, 30, 0x11},
{1280, 720, 15, 0x16},

{1024, 768, 30, 0x11},
{1024, 768, 15, 0x23},

{720, 576, 30, 0x1E},
{720, 576, 15, 0x23},

{720, 480, 30, 0x1E},
{720, 480, 15, 0x23},

{640, 480, 30, 0x1E},
{640, 480, 15, 0x23},

{320, 240, 30, 0x1E},
{320, 240, 15, 0x23},

{176, 144, 30, 0x1E},
{176, 144, 15, 0x23},
};

Can you please provide the more information?

0 Kudos
Reply
1,487 Views
joanxie
NXP TechSupport
NXP TechSupport

you don't need change escape clock, as I mentioned before, you need check your FPGA side clock, if could, pls measure the mipi  clock  by oscilloscope to check if correct or not I also attached the mipi guide to reference

0 Kudos
Reply
1,450 Views
shrithi
Contributor I

After correcting the FPGA clock, I am able to get the data with the following configuration.

assigned-clock-rates = <360000000>, <72000000>;

Can the resolution of 3056x3056 be supported by imx8 mipi-csi2 and ISI?

0 Kudos
Reply
1,483 Views
shrithi
Contributor I

When we measured clock using CRO(oscilloscope) and clock is 500MHz for FPGA with double data rate.

0 Kudos
Reply
1,454 Views
shrithi
Contributor I

In our case FPGA is the TX for MIPI, When we did probe clock using oscilloscope, the clock observed is 500MHz.

The below clock configuration done in device-tree
 assigned-clocks = <&csi0_core_lpcg 0>,
                     <&csi0_esc_lpcg 0>;
 assigned-clock-rates = <200000000>, <360000000>;

Tested with below configuration
number of data lanes - 4
resolution - 1920x1080@30fps
Data format - RGB888
1 pixel per clock
double data rate

FPGA Mipi TX IP configured with 1 pixel per clock will operate with a esc clock frequency of 180MHz and above.
FPGA Mipi TX IP configuration with 4 pixels per clock will operate with a esc clock frequency of 360MHz.
Can you provide an explanation for how this is changing?

We tested ov5640 camera with default configuration using 2 lanes and its working. When we did probe clock using oscilloscope, the clock observed is 24MHz. Here everything is working fine.

One more observation is streaming is happening with 15fps hs_setting value, i.e, 0x10. If I give below command the it is showing 30fps
v4l2-ctl -d /dev/video0 --set-fmt-video=width=1920,height=1080,pixelformat=RGB3 --set-parm=15 --stream-mmap
Frame rate set to 15.000 fps
[ 201.417005] bypass csc
[ 201.419426] input fmt RGB4
[ 201.422509] output fmt RGB3
<<<<<<<<<<<<<<<<<<<<<<< 30.03 fps
<<<<<<<<<<<<<<<<<<<<< 30.03 fps

I have confusion about esc clock and hs_setting value. So can you please provide us more information?
The severity of this case is high. Can you provide me with the solution as soon as possible?

0 Kudos
Reply
1,916 Views
joanxie
NXP TechSupport
NXP TechSupport

do you use imx8qm? and pls share dtsi files your current dts includes, I need check how you set mipi csi

0 Kudos
Reply