Hello,
I'm using MFRC522 for Mirfare and DESFire feature implement on reader without issue. Now, I prepare to implement Mifare Plus S and DESFire EV2 on MFRC522 chip also. Can MFRC522 use these security method? If yes, where I can get these sample code?
Thank you.
Hello,
Unfortunately. MFRC522 is an old product, so we don't have any sample code for this device. Please move to MFRC630 for a better support.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Thanks for the reply.
May I know where I can get MFRC630 sample code? In addition, is the sample compatible to MFRC522? Since I may use the same firmware on both of them.
Hello TaylorTJ,
I work with MFRC630 too. Did you finally get the sample code for DESFire EV2?
Thank you.