hi all,
I am using the ds26521 audio chip, in that i need to configure the T1 mode can any one help me with any basic settings on how to configure the T1 mode, is there any open source code is available, if so plz share the link
Thanks,
shan
已解决! 转到解答。
The case is put in DSC group, can you tell me the processor you are using to interface with DS26521? the StarCore or DSC family, do you use DSP5685x family? I think you should interface Ds26251 with SSI rather than SPI.
The case is put in DSC group, can you tell me the processor you are using to interface with DS26521? the StarCore or DSC family, do you use DSP5685x family? I think you should interface Ds26251 with SSI rather than SPI.