Cannot write firmware to RDDRONE-FMUK66

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot write firmware to RDDRONE-FMUK66

685 次查看
Mr_Maxwell
Contributor I

I have been able to write firmware to the RDDRONE-FMUK66 board, I have tried using the segger debugger and it is able to recognise the board but it cannot connect.

In addition when I try to upgrade the firmware using qgroundcontrol it does not work either, I get the following message:

Found device: PX4 FMUK66 v3.x

Connected to bootloader:

Version: 5

Board ID: 28

Flash size: 2072576

Plug in your device via USB to start firmware upgrade.

Downloading firmware...

From: http://px4-travis.s3.amazonaws.com/Firmware/stable/nxp_fmuk66-v3_default.px4

Download complete

MAV_AUTOPILOT = 12

Successfully decompressed parameter_xml

Successfully decompressed airframe_xml

Successfully decompressed image

Erasing previous program...

Error: Erase failed: Send Command: Command failed: 0x13 (PROTO_INVALID)

Upgrade cancelled

0 项奖励
回复
1 回复

673 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Maxwell,

We have a tutorial to program FMUK66 for first use. Please see this link: https://nxp.gitbook.io/hovergames/userguide/programming

Also you can use Segger debugger in case the board is bricked or to program it for the first time as well. https://nxp.gitbook.io/hovergames/developerguide/program-software-using-debugger

Best regards,

Felipe

0 项奖励
回复