Hello!
I am currently using LS1021ATSN-PA board, and I am using the Real-time Edge Software V2.4.
And I tried a command for configuring the tc qdisc taprio on the interface eth0 of the board.
But when I tried a command below,
tc qdisc add dev eth1 parent root taprio \
num_tc 8 \
map 0 1 2 3 4 5 6 7 \
queues 1@0 1@1 1@2 1@3 1@4 1@5 1@6 1@7 \
base-time 0 \
sched-entry S 80 50000 \
sched-entry S 40 50000 \
sched-entry S 3f 300000 \
flags 2
it prints out an error "RTNETLINK answers: Operation not supported".
Can I know the reason why it doesn't work, and how I can fix the problem?
Thank you, all!
Dear NXP team,
The current issue is that the eth3, eth4, and eth5 interfaces either do not exist or are not being recognized.
Additionally, there are no related messages about these network drivers appearing during the booting process.
Could you please check the network drivers and configurations?
<4>[ 0.427007] ahci-qoriq 3200000.sata: supply target not found, using dummy regulator
<6>[ 0.427214] ahci-qoriq 3200000.sata: AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl platform mode
<6>[ 0.427229] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc
<4>[ 0.427256] ahci-qoriq 3200000.sata: port 0 is not capable of FBS
<6>[ 0.428971] scsi host0: ahci-qoriq
<6>[ 0.429525] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 44
<6>[ 0.442840] tun: Universal TUN/TAP device driver, 1.6
<6>[ 0.443297] CAN device driver interface
<6>[ 0.448222] bgmac_bcma: Broadcom 47xx GBit MAC driver loaded
<6>[ 0.463645] fsl-gianfar soc:ethernet@2d10000: enabled errata workarounds, flags: 0x4
<6>[ 0.474714] fsl-gianfar soc:ethernet@2d10000 eth0: mac: b2:81:62:f2:95:bf
<6>[ 0.474725] fsl-gianfar soc:ethernet@2d10000 eth0: Running with NAPI enabled
<6>[ 0.474732] fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[0]: 256
<6>[ 0.474740] fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[1]: 256
<6>[ 0.474748] fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[0]: 256
<6>[ 0.474755] fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[1]: 256
<6>[ 0.475350] fsl-gianfar soc:ethernet@2d50000: enabled errata workarounds, flags: 0x4
<6>[ 0.486323] fsl-gianfar soc:ethernet@2d50000 eth1: mac: 72:df:f6:8f:1e:94
<6>[ 0.486333] fsl-gianfar soc:ethernet@2d50000 eth1: Running with NAPI enabled
<6>[ 0.486339] fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[0]: 256
<6>[ 0.486347] fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[1]: 256
<6>[ 0.486355] fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[0]: 256
<6>[ 0.486362] fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[1]: 256
<6>[ 0.487885] fsl-gianfar soc:ethernet@2d90000: enabled errata workarounds, flags: 0x4
<6>[ 0.498893] fsl-gianfar soc:ethernet@2d90000 eth2: mac: ce:b2:95:59:53:f4
<6>[ 0.498904] fsl-gianfar soc:ethernet@2d90000 eth2: Running with NAPI enabled
<6>[ 0.498910] fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[0]: 256
<6>[ 0.498918] fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[1]: 256
<6>[ 0.498925] fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[0]: 256
<6>[ 0.498933] fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[1]: 256
root@ls1021atsn:~# ip link show
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
2: can0: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10
link/can
3: can1: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10
link/can
4: can2: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10
link/can
5: can3: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10
link/can
6: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP mode DEFAULT group default qlen 10
link/ether b2:81:62:f2:95:bf brd ff:ff:ff:ff:ff:ff
7: eth1: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc mq state DOWN mode DEFAULT group default ql0
link/ether 72:df:f6:8f:1e:94 brd ff:ff:ff:ff:ff:ff
8: eth2: <BROADCAST,MULTICAST> mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/ether ce:b2:95:59:53:f4 brd ff:ff:ff:ff:ff:ff
9: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/sit 0.0.0.0 brd 0.0.0.0
root@ls1021atsn:/proc# ethtool eth3
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
No data available
root@ls1021atsn:/proc# ethtool eth4
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
No data available
root@ls1021atsn:/proc# ethtool eth5
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
netlink error: no device matches name (offset 24)
netlink error: No such device
Would you please address your current problem in a new thread?
First of all, it is need to be clear about the ls1021atsn hardware structure. As below. See attached picture 1. LS1021 internal link to the SJA1105. Ethx shows in Linux are the ports eth0/eth1 which links to ls1021. It only supports 1 RX ring and 1 TX ring per CPU. It is not support the TSN function. We called theses ports are the ethernet port as end station.
Thank you for your reply. Then I used the interface eth2, connected to a host. And I configured an IP address using ifconfig tool to the eth2 port, but I even couldn't ping to the host connected to the port. It printed out "Destination host unreachable". How can I fix this? I can't use the port eth2 for networking now.
eth2 is the port connecting to SJA1105, this port only has internal connection, no external connection, the user cannot use it.
I am not clear about your "internal connection only". The LS1021ATSN-PA switch has 6 physical ports. And I think the first 2 ports are normal ethernet ports, and the others are not But, because it is a networking device, I think an user have to be able to use all of the ports, and I want to use all of them, as well.
I wonder how I can do some TSN demonstrations by connecting some hosts to LS1021ATSN-PA switch. If I am right, you are saying that I can't use the other 4 ports for networking, and the 2 ports are for normal ethernet only, not for TSN.
If there is a way that I can do some networking with the other 4 ports, please tell me. In the picture below from the LS1021ATSN part of the Real-time Edge Software UG, it is demonstrated that the 4 ports other than normal ethernet ports, which are "SWP2 ~ SWP 5" from the picture, can be connected to external hosts and communicate.
So, please tell me how I can do this.
You can use swp2-swp5 to implement TSN networking features, use eth0 and eth1 to do normal networking application.
eth2 connects to sja1105 switch, there is no external PHY connecting to eth2, so it cannot be connected to the external networking.
But there are no interfaces named "SWX" for Real-Time Edge Software v2.4 which I am using. For using those interfaces, do I have to use the OpenIL?
Also, is it possible to use the interfaces in the same way as normal ethernet ports as eth0 and eth1 with which I can do some external networking?
Can you get similar result as the following?
[root@LS1021ATSN ~] # bridge link
6: eth0: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 master br0 state disabled priority 32 cost 100
7: eth1: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 master br0 state disabled priority 32 cost 100
10: swp5@eth2: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 master br0 state disabled priority 32 cost 100
11: swp2@eth2: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 master br0 state disabled priority 32 cost 100
12: swp3@eth2: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 master br0 state forwarding priority 32 cost 4
13: swp4@eth2: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 master br0 state disabled priority 32 cost 100
[root@LS1021ATSN ~] # ifconfig
br0 Link encap:Ethernet HWaddr A6:68:4A:23:E8:F5
inet6 addr: fe80::a468:4aff:fe23:e8f5/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:26 errors:0 dropped:0 overruns:0 frame:0
TX packets:33 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3508 (3.4 KiB) TX bytes:6114 (5.9 KiB)
eth0 Link encap:Ethernet HWaddr 00:04:9F:EF:06:06
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Base address:0xc000
eth1 Link encap:Ethernet HWaddr 00:04:9F:EF:07:07
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Base address:0xa000
eth2 Link encap:Ethernet HWaddr 00:04:9F:EF:08:08
inet addr:169.254.176.8 Bcast:169.254.255.255 Mask:255.255.0.0
inet6 addr: fe80::204:9fff:feef:808/64 Scope:Link
UP BROADCAST RUNNING PROMISC MULTICAST MTU:1504 Metric:1
RX packets:26 errors:0 dropped:0 overruns:0 frame:0
TX packets:93 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3976 (3.8 KiB) TX bytes:14538 (14.1 KiB)
Base address:0xe000
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:40 errors:0 dropped:0 overruns:0 frame:0
TX packets:40 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3040 (2.9 KiB) TX bytes:3040 (2.9 KiB)
swp2 Link encap:Ethernet HWaddr 00:04:9F:EF:08:08
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
swp3 Link encap:Ethernet HWaddr 00:04:9F:EF:08:08
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:26 errors:0 dropped:0 overruns:0 frame:0
TX packets:33 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3508 (3.4 KiB) TX bytes:6114 (5.9 KiB)
swp4 Link encap:Ethernet HWaddr 00:04:9F:EF:08:08
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
swp5 Link encap:Ethernet HWaddr 00:04:9F:EF:08:08
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
[root@LS1021ATSN ~] # ifconfig br0 1.1.1.2
[root@LS1021ATSN ~] # ping 1.1.1.1
PING 1.1.1.1 (1.1.1.1) 56(84) bytes of data.
64 bytes from 1.1.1.1: icmp_seq=1 ttl=64 time=0.683 ms
Yes, please provide Linux Kernel booting up log if the problem persists.