Can we use lwip's latest version 2.1.2 in LPCopen's webserver example?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use lwip's latest version 2.1.2 in LPCopen's webserver example?

389 Views
vishakhadakhane
Contributor III

Hello , I am using LPCxpresso and recently working on building SNMP agent . I am using LPCopen's webserver  example . And in that project there is a lwip folder which contains some SNMP files such as snmp.h ,snmp_asn1.h ,snmp msg.h etc. Recently i got to know that the version of lwip used in this example is 1.4.1, So can I replace this with the new version available and build the SNMP agent?

1 Reply

315 Views
soledad
NXP Employee
NXP Employee

Hi, 

For lwip version, yes it is possible to change the version.  You can look at this file for the list of application changes required between different lwIP versions.

Regarding SNMP, unfortunately, we don't have implemented it. Sorry for any inconvenience that may cause.


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------