Can I use a lower version of the eMMC chip than mpc8309 requires?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use a lower version of the eMMC chip than mpc8309 requires?

426 Views
RyongHa
Contributor I

Hi all

 

i want to use eMMC chip on my mpc8309 

but the mpc8309 datasheet writen : 

" Compatible with the MMC System Specification Version 4.2"

and eMMC datasheet writen :

"Compliant with eMMC Specification Ver.4.4, 4.41, 4.5, 5.0"

 

my best bet is to use a matching version of the chip

but first I want to know if this is possible

 

has anyone tried this?

 

thank for read this.

0 Kudos
Reply
0 Replies