Hi this is reg CBTL02043B IC .I was confused about DC LEVELS in datasheet.In datasheet they are telling SEL, XSD pins is 3.3V. But again input voltage for diffrential pins is 0 to 2V.but what is the range of each A0,1_P,A0_N,B0,1_Ppins support.right now what is the correct voltage needs to give for these differential pins.
Hello Varalakshmi,
The limit of the signal voltage level to switch pins (A/B/C) is below 2.4V max as shown in the datasheet on VI (input voltage) for differential pins.
Have a great day,
Paulina