CBTL02043B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CBTL02043B

634 次查看
varalakshmi_gop
Contributor I

Hi this is reg CBTL02043B IC .I was confused about  DC LEVELS in datasheet.In datasheet  they are telling SEL, XSD pins is 3.3V. But  again input voltage for diffrential pins is 0 to 2V.but what is the range of each A0,1_P,A0_N,B0,1_Ppins support.right now what is the correct voltage needs to give for these differential pins.pastedImage_1.png

0 项奖励
回复
1 回复

575 次查看
lisettelozano
NXP Employee
NXP Employee

Hello Varalakshmi,

The limit of the signal voltage level to switch pins (A/B/C) is below 2.4V max as shown in the datasheet on VI (input voltage) for differential pins. 

Have a great day, 

Paulina

0 项奖励
回复