CAN TJA1145AT/0Z & TJA1145AT/FD/0Z Essentially different

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN TJA1145AT/0Z & TJA1145AT/FD/0Z Essentially different

Jump to solution
291 Views
Louis1916
Contributor II

Customer feedback they use CAN TJA1145AT/0Z & TJA1145AT/FD/0Z,It was all used according to the CAN FD function, and there were no problems。Therefore, what is the specific difference between FD and FD in model naming。There are still differences from the specifications, as shown in the figure。Thanks!

微信图片_20240605111320.png

0 Kudos
Reply
1 Solution
276 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Louis,

please refer to the section 7.3.2 in the TJA1145A datasheet. Depending on the CFDC bit setting the  TJA1145AT and the TJA1145AT/FD will behave same (CFDC=0=>error counter increments) or (CFDC=1) the TJA1145AT/FD will ignore the CAN FD frames=>error counter decrements.

JozefKozon_0-1717569894265.png

JozefKozon_1-1717570002324.png

With Best Regards,

Jozef

 

View solution in original post

1 Reply
277 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Louis,

please refer to the section 7.3.2 in the TJA1145A datasheet. Depending on the CFDC bit setting the  TJA1145AT and the TJA1145AT/FD will behave same (CFDC=0=>error counter increments) or (CFDC=1) the TJA1145AT/FD will ignore the CAN FD frames=>error counter decrements.

JozefKozon_0-1717569894265.png

JozefKozon_1-1717570002324.png

With Best Regards,

Jozef