Are the PCA9671 I/O cold sparing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are the PCA9671 I/O cold sparing?

519件の閲覧回数
pete_scott
Contributor II

Hello,

The PCA9671 datasheet states that the input/output pins are "5 Volt tolerant".  Is there any issue with connecting an I/O to 3.3 Volts when VDD is not powered?

I note that the input voltage is speccified to a maximum of 5.5 Volts with no reference to the VDD pin.  However, I can't find figures for the I/O leakage current when the device is not powered, and don't want to take the answer from the absolute maximum values alone.

Many thanks!

Pete

0 件の賞賛
返信
1 返信

460件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Pete,

I need to consult this with our design team and will update this thread as soon as I have their feedback.

 

Thanks for your patience.

 

Best regards,

Tomas

0 件の賞賛
返信