About the mpc5604 emios interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the mpc5604 emios interrupt

Jump to solution
1,142 Views
Aboutthempc5604
Contributor I

I see every emios have 14 interrupt, but I in technical  manualsDidn't find what they are interrupt also didn't find how the
set up interruption.

0 Kudos
Reply
1 Solution
685 Views
TomE
Specialist II

MPC5406 Reference manual

 

Table 16-10. Interrupt vector table (continued)

 

Interrupts are on EMIOS_GFR[F0,F1] to EMIOS_GFR[F26,F27] for eMIOS_0 and eMIOS_1.

 

24.4.3.2.2 eMIOS Global FLAG (EMIOSGFLAG) Register

 

Details the 28 Flag bits.

 

24.4.3.2.8 eMIOS UC Control Register (EMIOSC[n])

 

Has the DMA and FEN bits to enable FLAG bit setting to cause an interrupt.

 

This is a very complicated module. I'd look for some sample code (I don't use this chip).

 

Tom

 

View solution in original post

0 Kudos
Reply
1 Reply
686 Views
TomE
Specialist II

MPC5406 Reference manual

 

Table 16-10. Interrupt vector table (continued)

 

Interrupts are on EMIOS_GFR[F0,F1] to EMIOS_GFR[F26,F27] for eMIOS_0 and eMIOS_1.

 

24.4.3.2.2 eMIOS Global FLAG (EMIOSGFLAG) Register

 

Details the 28 Flag bits.

 

24.4.3.2.8 eMIOS UC Control Register (EMIOSC[n])

 

Has the DMA and FEN bits to enable FLAG bit setting to cause an interrupt.

 

This is a very complicated module. I'd look for some sample code (I don't use this chip).

 

Tom

 

0 Kudos
Reply