Hi Robert,
If the BDM appears to work otherwise it is possible that I simply have the wrong SDID(partid) for the device. I don't have a XDT256 to check this. The BDM works fine with a XDT512. I believe these are the same chip as, according to the device manual, they have the same partid. This might have changed.
When you ask the programmer to detect the target does this fail with the failed to connect dialogue? If this is not the case could you let me know what number appears on the programmer dialogue (under the device name).
bye
Hi pgo,
Thanks for the reply.
When I click the “Detect Device” tab I get a message “No matching device”. The “Filter by chip ID = (C001).
If I uncheck the “Filter by chip ID” I get the drop down list of MCU’s including the XDT256. I select this and try to program the device.
This results in a message box: “Selected target device does not agree with detected device. (Unable to read / confirm CHIP_ID)”
If I select “Verify” then the verify works perfectly fine. (The MCU has previously been programmed with a Cyclone Pro).
Note that I am using the USBDM in stand-alone mode, and it works perfectly fine on 9S12P128 and 9S12DG128 variants.
Thank you.
From: pgo
Sent: Friday, January 31, 2014 9:14 PM
To: Robert Richardson
Subject: Re: - USBDM won't program MC9s12xdt256
USBDM won't program MC9s12xdt256
reply from pgo in OSBDM and TBDML - View the full discussion
Hi Robert,
Yup - it doesn't have the correct SDID. I missed that one in the data sheet.
Quick fix is to edit the file C:\Program Files (x86)\pgo\USBDM 4.10.6.110\DeviceData\hcs12_devices.xml that describes the devices.
Locate the entry for MC9S12XDT256 and add the following line below the similar lines:
<sdid value="0xC001" /> |
bye