USBDM, the RS08 KA8 and Vpp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USBDM, the RS08 KA8 and Vpp

跳至解决方案
8,960 次查看
markslFS
Contributor I

Dear pgo,

 

I don't know if the problem is in the BDM code, or elsewhere, but I have found that the USBDM does not drop the 12V Vpp after programming the RS08KA8.

 

I have got around it by adding FLASH12V_OFF() after VPP_OFF() in CmdProcessing.h after line 893,

"case CMD_FLASH_DLEND:"

 

            VPP_OFF();     // Turn Proramming voltage off            FLASH12V_OFF();// KAM Turn off charge pump

 The code is inserted twice.

 

Thanks,

Kevin

 

标记 (2)
0 项奖励
回复
1 解答
1,537 次查看
pgo
Senior Contributor V

Dear marksl,

 

I'll look at this in more detail later - I'm rather busy at the moment. 

 

Some comments:

 

Even with a blocking diode you may still have voltage fed through the pull-up resistors on the HC125 outputs if there is no load?

 

The HC125 is not a suitable device as it is not rated to have 5V in/out when running on a lower rail voltage.  A 74LC125A is pin compatible and can be used instead.  You can use the two spare gates to eliminate Q2 if RST_IN and RST_OUT are separated.

 

I can only suggest removing the HC125 and confirm that the problem goes away, then try without the pull-ups.

 

bye

 

Message Edited by pgo on 2009-04-18 05:18 PM

在原帖中查看解决方案

0 项奖励
回复
10 回复数
1,537 次查看
pgo
Senior Contributor V

Dear marksl.

 

This shouln't be necessary.  VPP_OFF() should turn off the Vpp voltage via an isolating transistor (BSS84).  FLASH12V_OFF() turns off the charge pump and should be redundant. It's there really as a safety precaution so that Vpp=12V can't be applied to other than RS08 devices (the pump is off for all other devices).

 

Can I just check is this the JB16 or JMxx version of USBDM?  If you let me know I'll check these in case I've broken something in a software revision. 

 

In the mean time, check the above switching transistor or the port pin controlling it.  If it is not working correctly there may still be problems with excessive current flow when resetting the target.

 

bye.

0 项奖励
回复
1,537 次查看
markslFS
Contributor I

Dear pgo,

 

I am using the JB16 version.

 

I have also discovered that I made a mistake transcribing your circuit - it seems I swapped drain and source of MOSFET Q3. I don't know what effect that has, perhaps this is what is causing the 12V to still be present when VPP is turned off.

 

The circuit works at present, but for two issues:

1) I had to include the above mentioned code to fully turn off Vpp after flash write (on the KA8), and

2) I can't get Vdd to turn off properly. There is always at least 3V present. I use the USBDM test program, with commands "debug 9", "debug 10", etc.

 

Sincerely,

Kevin

0 项奖励
回复
1,537 次查看
pgo
Senior Contributor V

Dear marksl,

 

Transposing D & S will cause the 12V to be always present since the D-S diode will be forward biased.  Best to fix this :smileysad:

 

The 3V should be switchable- check that the control input to the  regulator is changing when Vdd is switched on and off using the debug commands.

 

Good luck.

 

bye

 

 

0 项奖励
回复
1,537 次查看
markslFS
Contributor I
Dear pgo,

I've fixed Q3's drain and source, and confirmed that your original code removed 12V from Vpp after programming. I'll probably leave the mod in place - there is no need for the charge pump to run when it's not needed.

I've discovered that the 3V present on Vdd_BDM is coming from the Philips 74HC125N buffer I'm having to wire onto the board (I don't have any 74LVC2G125D's yet). For some reason, that IC is outputting 3V from its Vcc pin. I can try replacing the Philips version with a TI version, and see if anything changes. Hopefully the 74LVC2G125D won't present the same problem.

My board is looking a little like a crows nest with the corrections and mods I've had to implement. Perhaps I should upload a picture sometime...

I've implemented the USBDM as a plugin module onto a JB16 template board. This means I can re-use the JB16 template board design.

Once again, thanks for your efforts,

Kevin
Message Edited by marksl on 2009-02-19 11:06 AM
0 项奖励
回复
1,537 次查看
markslFS
Contributor I
Dear pgo,

marksl wrote:

I've discovered that the 3V present on Vdd_BDM is coming from the Philips 74HC125N buffer I'm having to wire onto the board (I don't have any 74LVC2G125D's yet). For some reason, that IC is outputting 3V from its Vcc pin. I can try replacing the Philips version with a TI version, and see if anything changes. Hopefully the 74LVC2G125D won't present the same problem.


I recently placed a diode between the Vcc rail and the Vcc pin on the HC125 buffer, and the Vdd_BDM still would not drop to 0V. If I use my own inserted debug commands to force the BDM_DRV and BDM_OUT to known levels, I can get Vdd_BDM to 0V.

 

To repeat: I can raise Vdd_BDM to 3.3V and 5V, but I can not force it back to 0V without manually resetting the BDM_* control lines.

 

I have attached my schematic.

 

Do you have any suggestions/comments?

 

Sincerely,

Kevin

 

Message Edited by marksl on 2009-04-16 03:24 PM
Message Edited by t.dowe on 2009-10-26 04:49 PM
0 项奖励
回复
1,538 次查看
pgo
Senior Contributor V

Dear marksl,

 

I'll look at this in more detail later - I'm rather busy at the moment. 

 

Some comments:

 

Even with a blocking diode you may still have voltage fed through the pull-up resistors on the HC125 outputs if there is no load?

 

The HC125 is not a suitable device as it is not rated to have 5V in/out when running on a lower rail voltage.  A 74LC125A is pin compatible and can be used instead.  You can use the two spare gates to eliminate Q2 if RST_IN and RST_OUT are separated.

 

I can only suggest removing the HC125 and confirm that the problem goes away, then try without the pull-ups.

 

bye

 

Message Edited by pgo on 2009-04-18 05:18 PM
0 项奖励
回复
1,537 次查看
markslFS
Contributor I

Dear pgo,

 

It works!

 

Thanks, it seems that the problem was with the HC125 buffers. Using the LVC2G125 everything works fine - I've got full control over Vdd_BDM - 0, 3.3 and 5V.

 

Sincerely,

Kevin

 

 

 

0 项奖励
回复
1,537 次查看
markslFS
Contributor I

Dear pgo,

 

With the HC125 removed (or even just un-powered), the problem is no longer present. Which pullups are you referring to? R1 & R17?

 

I shall make up another board using a LVC2G125 I recently received from Farnell. Hopefully the problem is only in the buffer, and not in the rest of circuitry.

 

I appreciate your attention.

 

Sincerely,

Kevin

0 项奖励
回复
1,537 次查看
pgo
Senior Contributor V

Dear marksl,

 

R17 would be the one I had in mind.

 

bye

0 项奖励
回复
1,537 次查看
markslFS
Contributor I

Dear pgo,

 

Funny, but it seems like I left off R17 during transcription...

 

I'm building a new board today. I'll keep you informed.

 

Thanks,

Kevin

0 项奖励
回复