USBDM can't unsecure MKE04Z128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM can't unsecure MKE04Z128

ソリューションへジャンプ
1,617件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

in my program,I secure MKE04Z128.now I want to reprogram the chip.I find I failed.

pastedImage_1.png

I think USBDM can't unsecure MKE04Z128.

Is this a bug?

タグ(2)
0 件の賞賛
返信
1 解決策
1,068件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

II have confirmed the problem with a MKE04Z8. I will have a look at this and see if I can find the reason.

bye

PS. It appears that it is probing a secured device that is upsetting the chip.

Try the following:

  • Unplug the programmer to power cycle the chip
  • Plug in the programmer.
  • Manually select the correct device
  • Select the unsecured option
  • Select Mass erase
  • Program an image to the device.

The above worked for me.

bye

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,069件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

II have confirmed the problem with a MKE04Z8. I will have a look at this and see if I can find the reason.

bye

PS. It appears that it is probing a secured device that is upsetting the chip.

Try the following:

  • Unplug the programmer to power cycle the chip
  • Plug in the programmer.
  • Manually select the correct device
  • Select the unsecured option
  • Select Mass erase
  • Program an image to the device.

The above worked for me.

bye

0 件の賞賛
返信
1,068件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

USBDM still can't unsecure MKE04Z128 . do you have other way to resolve the question?

0 件の賞賛
返信
1,068件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

I'm sorry but I've been unable to re-produce your problem.

The MKE devices require a slightly different unsecure sequence which does interfere with the device auto-detection.

However, manually selecting the device and programming with mass-erase as described above seems to work fine with the several devices I tried.

Is there anything particular about the program in the chip you are using?

Note: I do not have a MKE04Z128 to check with only MKE02, MKE06  and MKE04 in a different size.

bye

0 件の賞賛
返信
1,068件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

I download the latest version usbdm . I try it and it works. thank you.

bye

0 件の賞賛
返信
1,068件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

A new question comes out. I can debug MKE04z128 in cw10.6,but I can't use ARM programmer to download my app into MKE04Z128. when I try to download it,the picture shows the error.

I don't find the question in other KE02 series.

0 件の賞賛
返信