USBDM can't be used in freescale KSDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USBDM can't be used in freescale KSDK

1,104 次查看
wangbaode
Contributor IV

hi pgo,

I want to use usbdm to debug demo in ksdk. but i'm failed. the error is in the picture.

bye

标记 (3)
0 项奖励
4 回复数

876 次查看
pgo
Senior Contributor V

Hi Wang,

Have you updated the firmware to the version included with USBDM?

This looks like a problem with it expecting a different response on register read failure.

bye

0 项奖励

876 次查看
wangbaode
Contributor IV

Hi pgo,

According to your response , I update the firmware and retry it . but It's failed to debug ksdk project . If i new a project in kds , usbdm can debug the projcet .

you can download the freescale sdk from the link and try it.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_SDK&fsrch=1&sr=8&pageNum=%E4%...

0 项奖励

876 次查看
pgo
Senior Contributor V

Hi Wang,

I don't have a twrk60d100 to try out your example, however I was able to load several of the other demonstrations for other boards without significant problems.

When I tried the flash_demo_twrk60d100m example with a TWR-K60N512 it did load but did not execute correctly as it is the wrong CPU.

bye

0 项奖励

876 次查看
wangbaode
Contributor IV

OK,thank you

0 项奖励