Dear All,
USBDM has been updated to V4.9.4.
Please post any queries on this version in this thread,
Information available at: SourceForge
bye
Note
BDM History4.9.4 (April 2012) -
Hello PGO, I tried it and failed:
http://img594.imageshack.us/img594/4425/fm1v.png
http://img826.imageshack.us/img826/295/fm2v.png
That was in a WinXP 32-bit virtual machine, my main OS is Win7 64-bit
However I unistalled FreeMaster, deleted extra files in its program files, reinstalled it with "stock" USBDM 4 drivers (v4.4) and now it's working !
http://img716.imageshack.us/img716/8867/fm3t.png
Here's the comms config dialog:
I wonder is there any performance or feature extra in v4.9 plugin ?
hello PGO
I use MC13233(HCS08QE) and can Detect it (4028)
but I can not write image file to it .
error message as attach file.
Programming of the target flash failed!
Reason: Program data not within target Flash Memory
can you give me some idea.
Thank you.
Hi,
I'm unable to get the driver to recognize a USBDMLT. My OS is Windows Vista Business SP 2.
The Device Manager shows
libusb (WinUSB) devices
! USBDM BDM Interface
This device cannot start. (Code 10)
The BDM Firmware Update application does not see the USBDMLT nor does Zadig.exe
Any suggestions on how to get the USBDMLT recognized by the driver?
Thanks
Dear Swood,
Things to try (rather obvious):
Not much help really. I have used similar BDMs on Vista (briefly) and they seemed to work OK.
bye
Hi Peter,
First of all, I want to thank you for your excellent work in implementing the new features of v4.9-- it is a huge improvement to a very useful tool!
We have been testing it with multiple targets, with great success, but have been unable to program 9S12E256 devices. The E256 is not recognized by the standalone programmer, so we tried adding the parameters to the XML file, without any success. I'm guessing there is another file that needs to be updated? The chip ID for E256 is 5002, but the programmer reports "Programming of the target flash failed! Reason: Execution of TCL script returned an error".
If you could point me in the right direction to resolve this, I would be grateful!
Carl
Dear Carl,
The difficulty of adding a device depends upon how similar to an existing device the new device is.
A device requires the following:
The first two of the above are located in the HCS12 directory under the Device_data Directory.
I believe that the E256 is very similar to the E128 so should be able to use the same binary and TCL scripts and only require the XML to be changed - With one problem - There is a bug in the existing binary file that prevents programming if the flash block size is large. This bug would apply to the E256 device. There is a fix posted on Sourceforge. After applying this fix I believe the following device entry would work.
Please advise if it does.
Note: I am suprised by the particular error you are seeing since I would expect the 'standard' TCL script to work with this device. There may be something I am overlooking.
<device family="HCS12" name="MC9S12E256"> <clock type="External" /> <memory type="ram"> <memoryRange end="0x3FFF" start="0x0400" /> </memory> <memory pageAddress="0x0030" registerAddress="0x0100" type="flash" securityAddress="0xFF00" sectorSize="1024"> <securityInfoRef ref="HCS12-default-security-off" /> <securityInfoRef ref="HCS12-default-security-on" /> <memoryRange end= "0xBFFF" start= "0x8000" pageNo="0x30" /> <!-- Reset default 0x30? --> <memoryRange end="0x30BFFF" start="0x308000" /> <memoryRange end="0x31BFFF" start="0x318000" /> <memoryRange end="0x32BFFF" start="0x328000" /> <memoryRange end="0x33BFFF" start="0x338000" /> <memoryRange end="0x34BFFF" start="0x348000" /> <memoryRange end="0x35BFFF" start="0x358000" /> <memoryRange end="0x36BFFF" start="0x368000" /> <memoryRange end="0x37BFFF" start="0x378000" /> <memoryRange end="0x38BFFF" start="0x388000" /> <memoryRange end="0x39BFFF" start="0x398000" /> <memoryRange end="0x3ABFFF" start="0x3A8000" /> <memoryRange end="0x3BBFFF" start="0x3B8000" /> <memoryRange end="0x3CBFFF" start="0x3C8000" /> <memoryRange end="0x3DBFFF" start="0x3D8000" /> <memoryRange end="0x3EBFFF" start="0x3E8000" /> <memoryRange end="0x3FBFFF" start="0x3F8000" /> <memoryRange end= "0xFFFF" start= "0xC000" /><!-- Fixed 0x3F --> </memory> <sdid value="0x5000" /> <flashProgramRef ref="HCS12-MMCV4-FTS_2-flash-program" /> <note>Untested</note> </device>
bye
Thanks for your help!
I downloaded and applied your HCS12_Fixes of 5/21 and here's what happened:
It refused to erase flash, producing the error message: "Selected target device does not agree with detected device. (Unable to read/confirm CHIP_ID)".
I edited the devices XML file to use 5002 for the sdid value (instead of 5000). After that, erase worked fine, but I was unable to program any files into the chip ("Programming of the target flash failed! Reason: Program data not within target Flash Memory").
I added this line to the XML file:
<memoryRange end= "0x7FFF" start= "0x4000" /> <!-- Fixed 0x3E -->
and it now works.
Carl
Hi there.
I have some issue with the program, for example when I start to program the memory flash appears a message "Program data not within targe flash memory" but looking in to the file hcs12_devices.xml it is correct and the file it is correct because we use it with PE micro without any problem.
Although it see PE micro use Algorithm to program the device so my question is: could be algorithm problem or a memory issue
Regargs
Thanks for letting me know Carl.
I'm sorry I overlooked that you had indicated a partid of 0x5002 in your earlier posting. The data sheet only has 0x5000.
The memory regions were from the memory map in the data sheet but in the fine print it indicates it's a "useful" map rather than the one out of reset nor the one used by Codewarrior.
I've updated the update on Sourceforge.
bye
Hi there, I'm really pleased with the USBDM. Previously I used TBDML (also terrific) but had trouble on a new Netbook. The new USBDM works very well, however the netbook i need it for only has a 1024x600 screen and thus the bottom part of the standalone flasher program is not visible !! ( ie the bit that erases and flashes the device !!)
With an external (normal) monitor it's no problem, but I can't use it on site with the netbook's screen.
Would there be any chance of a build of the HC12 programmer application with, say , a wide layout rather than a tall layout?
I know it's a lame request but i would be grateful if there's a chance of it...
regards.
duaneM wrote:Hi there, I'm really pleased with the USBDM. Previously I used TBDML (also terrific) but had trouble on a new Netbook. The new USBDM works very well, however the netbook i need it for only has a 1024x600 screen and thus the bottom part of the standalone flasher program is not visible !! ( ie the bit that erases and flashes the device !!)
With an external (normal) monitor it's no problem, but I can't use it on site with the netbook's screen.
Would there be any chance of a build of the HC12 programmer application with, say , a wide layout rather than a tall layout?
I know it's a lame request but i would be grateful if there's a chance of it...
regards.
I've had this problem too would be nice to have it in a wide version for this small screen netbooks.
Hello PGO, I've still been having problems with Freemaster, as there's no visualization tools on CW v10.2 yet There's the most feasible way to do something similar. I use Win7 64-bit but have tried in WinXP 32-bit with same results:
Dear carloscuev,
I have not used Fremaster apart from doing a basic test.
I have just done a quick test and the BDM is detected etc with the current version of software and firmware but I have not tested it further.
I cannot open the image posted so I'm unsure if you are geting past the above stage.
bye
Thaks PGO, image is here:
http://img444.imageshack.us/img444/2239/58466333.png
I hope it's a minor setting I'm missing.
Dear carloscuev,
The error appears to be that it can't load the interface DLL (or something that the DLL depends on).
Can you check the Freemaster diretcory:
C:\Program Files\Freescale\FreeMASTER 1.3\plugins\bdm
and see if the following files are present:
usbdm.4.dll
libusb-1.0.dll
libstdc++-6.dll
libgcc_s_dw2-1.dll
If not please re-install the software and check the installation path being used to see if it is correct. It should detect FreeMaster automatically.
If that doesn't fix it you can copy the required files from the USBDM install directory and I will check the installer script.
bye
Dear PGO,
Is there any hope of being able to use your USBDM-CF design with other DSCs than the MC56F80xx devices, such as a MC56F8365, or do the MC56F83xx use entirely different programming algorithms?
With a MC56F8013 it works fine, but for a MC56F8365 with CW 10.2 it gives the attached error message ...
Many thanks!
Robert
Dear Jonca,
I'm sorry but it is unlikely that the MC56F8365 will be added in the near future. There are a couple of reasons. Firstly the chip is a bit different to the ones done and secondly I don't have acces to a chip to test so it would be a bit impractical to debug.
bye