Dear All,
USBDM has been updated to V4.6. This version adds support for Kinetis devices but please be aware that this has had minimal testing due to lack of devices to test with .
Please post any queries on this version in this thread,
Information available at: http://usbdm.sourceforge.net/
bye
Notes
Please note that these design are different from the Freescale OSBDM-JM60 design which was proceeding independently while I was doing the above designs
Hello pgo !
Here are the logs, please tell me if you need me to run anything else
Dear carlosuev,
That helps a lot. The error is occurring because the filename wildcards (*.*.*) are being expanded at the command line instead of being passed to the mergeXML program. This isn't a problem if there is only one matching wizard folder hence the simple fix of renaming all but the most recent wizard folder. The latest is the one with the highest number e.g. com.freescale.mcu.projectwizard_1.3.50.FSL_b02061 in your case.
I did test for this sitation under XP and it worked fine, so I think it must be something OS dependent. Could post details about which OS (incuding language) you are using?
In any case I will have to fix it but it would be better if I could reproduce the problem so that I can confirm it has been fixed.
bye
Hello pgo, I found a solution !
I checked the previous log file and noted this:
"C:\Program Files\Freescale\CW MCU v10.1\eclipse\plugins\com.freescale.mcu.projectwizard_1.*.*.*"
So I thought, the folder isnt fixed, it hopes to find only one matching folder using those wildcards !
I checked if I had 2 folders that could match and bingo !
I really dont know why I have 2 matching versions, I only installed CW v10.1 months ago for a Freescale Training with the KwikStik and a hole bunch of updates needed to be able to run the samples they gave us. I'm starting to use CW v10 because soon I'll be getting a bigger machine with more ram than a 32-bit system can handle, so I will be hopping on the 64-bit bandwagon !!
I renamed one of them with an extra character so it didnt match and voila! it worked, then made the same with the other one to have the 2 versions patched and voila again!
I needed to run "c:\Program Files\Freescale\CW MCU v10.0\eclipse\cwide.exe" -clean to get the new USBDM option in the project wizard.
If anyway you need me to run the previous precedure you told me, please tell me so, I'll be glad to help !!!
Thanks for your great support pgo !
Dear Carloscuev,
I'm glad you found a solution.
I would expect there to be more than one folder matching as that is one of the things that may occur if an update is applied. The matchXML.exe program is meant to cope with that and update all matching folders. It's failing on the first one for some reason. It would be good to know why.
I would appreciate you trying the above process to see if we can determine what is unusual about your original situation that is causing my program to fall over
The test case I tried had a 'pretend' folder matching yours and another later version folder but it displayed no errors.
The other problem with needing to run codewarrior with the -clean option will be fixed in the next version of the installer.
bye
Hello PGO, I tried the Tips for USBDM and didnt work.
Install log is here: http://escalalibre.com/usbdmInstall.log
Heres a screenshot of the folder, I checked path twice and I think it's correct, somehow installer could not find it
(http://img585.imageshack.us/img585/3738/freescalepath.png)
Thanks !
Dear carloscuev,
I'm pretty much stumped about what is going wrong.. The log file indicates the correct command is being executed with the correct parameters. The only way I've been able to get the particular error message you have seen is by intentionally using the wrong parameter (an illegal filename).
Anyway - I've attached a zip file containing a new version of the mergeXML.exe program. This has only very minor functional changes but now reports more fully what it is doing. I have also provided three command files that run the existing mergeXML and the new version with various options.
Please do the following:
Roughly, the command files do the following
Thanks
Hello PGO, I tried to install v4.7.0g and got this problem, I'm new to CW v10.1 but have to learn because I need to develop for RS08, I'm not sure what this problem causes.
I noticed that when creating a bareboard project when selecting connection theres no USBDM option, only Open Source BDM which I later edit to make it run, does the error advertised on the screenshot causes this problem?
Thank you very much PGO, your work is awesome.
Dear carloscuev,
You asked:
I noticed that when creating a bareboard project when selecting connection theres no USBDM option, only Open Source BDM which I later edit to make it run, does the error advertised on the screenshot causes this problem?
Yes is does. When installing for Codewarrior Eclipse, USBDM modifies the New Project Wizard files to add the USBDM options as shown in the help files screen grabs. For some reason this is failing in your case.
Things to try
Could you check that the directory indicated in the dialogue exists and is not empty.
bye
Hi PGO and Carloscuev,
I had the same problem with USBDM not appearing as an option in CW10.1 New Project Wizard (tried it both in XP 32bit and Windows 7 64 bit).
Running "c:\Program Files\Freescale\CW MCU v10.1\eclipse\cwide.exe" -clean fixed it.
Best regards,
Robert
Thanks Robert.
I think this is an unrelated problem to the one Carloscuev has - You didn't get the pop-up dialogue during the install?
The installer runs a similar command but there (were) some issues to getting things to happen in the correct order. It was running that step BEFORE modifying the XML files
The next :smileyalert: version will fix this.
bye
Hi PGO,
you are right, I did not get that error message popup ...
I just completed a prototype of your "deluxe" version, and all varieties of targets work fine.
I tried to find a solution that would allow the usbdm to plug directly onto the target boards without ribbon cables -- if there are no excessively high components nearby, it works well (except for the 0.05 pitch Kinetis connector where I couldn't find a suitable horizontal female header, so there it sits flat above the target ...)
Many thanks for all your terrific work !
Robert
pgo wrote:
You obviously don't have any problems doing SMT soldering!
Is this a single or double-sided board?
Hi PGO,
the components are all on one side and the routing is two-sided.
For the soldering I can't lay claim to great manual diligence because the place I get the prototype pcbs from (pcb-pool.com) supplies free solder paste stencils with every board -- with a converted toaster oven the assembly becomes easy ...
best regards,
Robert
Robert, nice board!
joncas wrote in part:I just completed a prototype of your "deluxe" version, and all varieties of targets work fine.
I tried to find a solution that would allow the usbdm to plug directly onto the target boards without ribbon cables -- if
Hi pgo
report a v4.7e version of the small problems.
Chip: MC9RS08KA1
Software: CW10.1
when use this:
const byte NVOPT_INIT @0x00003FFC = 0xFE;
after the download is complete, not complete FLASH encryption.
in test.s19 file
S1073FFCFEBC386E5D
work around:
use RS08_FlashProgrammer
Dear Mickey,
When used with Codewarrior, USBDM intentionally programs the device to an unsecured state (0x3FFC=0xFF) to allow debugging. It ignores any value in the image file. It doesn't seem advisable to change this.
As you have discovered, to do 'production' programming it is necessary to use the stand-alone programmer.
bye
Hi pgo
does the version support coldfire+ MCU?
Hi bluehacker,
It doesn't. I don't have any chips to experiment with and AFAIK they are not available. The only way I could obtain one would be to purchase a TWR-MCF51QM which would be a bit excessive .
bye
Dear PGO,
I wanted to ask if the changes between schematic version 2 and version 3 are documented anywhere? Apart from the addition of the serial interface which is listed in the changes, I noticed the JTAG_DRVR signal was added to control the enable lines of TDI, TMS and TCLK, and the two surge protectors Z1, Z2.
Where there other changes?
Then I wanted to ask about the need for pull-up resistors on the Kinetis targets. In the Freescale documentation it says TDI, TMS and TCLK are supposed to have pull-up resistors, but on the K40 in a 144 pin package I'm running short on pins and need to use the JTAG pins as touch sensor inputs in normal operation, which would not be possible with pull-ups. Depending on how the JTAG_DRVR is set, would the USBDM not drive those lines to the required levels without adding pull-up resistors?
Many thanks!
Robert