Dear All,
USBDM has been updated to V4.10.6.110
Please post any queries on this version to separate threads.
Documentation available at: SourceForge
Applications available at: SourceForge
Source code is available at: GitHub eventually.
bye
Note - Please note that these design are different from the Freescale OSBDM-JM60 design which was proceeding independently while I was doing the above design
USBDM consists of two components:
Hardware interfaces for various target devices
Software to support these interfaces. This includes:
Where applicable, the software is available for Windows and Linux.
Change History
V4.10.6.110 (February 2014) - This mainly concentrates on Eclipse support for Kinetis devices
Screen Shots
Hi, pgo:
I noticed that USBDM will support KEIL soon.
It;s really a great work to support KEIL. Some engineers and students like to use KEIL.
Have you finished partially work on some chip? I think I can do some test on KEIL and Kinetis.
Many thanks,
Best regards,
Tao Xue