USBDM 4.12.1.210 Unable to program MC9S12G128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM 4.12.1.210 Unable to program MC9S12G128

1,013件の閲覧回数
carlosjuarez
Contributor II

Hi pgo

I'm working with USBDM from Witztronics using WTUSBDM_CF_JM to program S9S12G128 but I have some issues for example when I tray to flash the memory program it says "Program data not within target flash memory" and the way I do it is fist program eeprom memory using erase mass option and for the flash program EraseSelective option.

EEprom.pngFlash.png

So I think it could be flash memory configuration issue because flash range start on 0x20000-0x3FFFF for S12G128 and hcs12_devices.xml and I don't see it where.

Flash range.pngDevice-xml.png

And the flash program it's correct because we use it with PEmicro and works well.

タグ(1)
0 件の賞賛
返信
0 返答(返信)