Hi,
I have a problem with installation of USBDM 4.10.6 package on Windows 7 32-bit. I have checked on two PCs with this operating system and it behaves the same. After window with installation options there is a popup:
I have 4.10.5b version and it was installed without a problem. Of course previous version was removed before attempting to install 4.10.6.
Regards,
adamb
解決済! 解決策の投稿を見る。
Hi adamb,
Yes I discovered this a little while ago. One of the DLLs used by the installation has a dependency on a MinGW library. This doesn't show up on my test machine as it has MinGW installed.
A corrected installer was uploaded a few hours ago.
bye
Hi adamb,
Yes I discovered this a little while ago. One of the DLLs used by the installation has a dependency on a MinGW library. This doesn't show up on my test machine as it has MinGW installed.
A corrected installer was uploaded a few hours ago.
bye
Hi pgo,
The 4.10.6a still not working on win7 and winXP. I tried more than 5 PCs with no success.
The 4.10.5b works fine!!!
Tested with hardware USBDM_JMxxCLD.
bye