OSBDM firmware?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OSBDM firmware?

6,370件の閲覧回数
FOLSOT
Contributor I
Hi,

Can you tell me where you find the firmware for the OSBDM project? :smileysad:
Taking advantage of the opportunity, you could say to me, which of versions OSBDM08 is the one that has less conflicts?

Thanks and  sorry english is not my mother language :smileyhappy:

Message Edited by FOLSOT on 2007-04-1807:20 PM

ラベル(2)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,024件の閲覧回数
joerg
Contributor II
Hi
The firmware can be found here:

http://forums.freescale.com/freescale/board/message?board.id=OSBDM08&message.id=2&view=by_date_desce...

and info about hardware here:

http://www.systech-gmbh.ch/indexHCS08System.html

If you have any questions feel free to ask me.

Saluti Joerg
0 件の賞賛
返信

1,024件の閲覧回数
FOLSOT
Contributor I
Thanks Joerg, Very useful answer, I build your version  is interesting and very complete. Exis any update in your schematics?   
Again thanks for all :smileyvery-happy:

Message Edited by FOLSOT on 2007-04-1811:18 PM

0 件の賞賛
返信

1,024件の閲覧回数
joerg
Contributor II
Hi Folsot

Until now i did not change the circuit. If i get some time I'd like to replace the ugly RC stuff on the BDM line with a clean solution. This requires hard and software changes. I actually am studying the listings of the firmware and have understood how it works, now i am thinking of a solution to integrate the power on reset function (detected by a comparator on the target power line).

Saluti Joerg
0 件の賞賛
返信

1,024件の閲覧回数
FOLSOT
Contributor I
Hi Joerg, thank you very much...
I hope to try change the ugly RC, if success I upload here.
Thanks
0 件の賞賛
返信