Hi all!
I'm using a MC13213 system-on-chip from Freescale in my undergratuate final project in college. But the problem is that I don't any hardware to burn/debug the code in the uc inside MC13213 (MC9S08GT) . I would like to know if I can use OSBDM with this particular chip to burn/debug my code inside CodeWarrior?
thanks in advance
Dear Danielt3,
I don't have a MC13213 module to test but it would appear from the Spec sheet that it has the standard BDM interface available. OSBDM is supported as a target for the MC9S08GT in Codewarrior so I would be surprised if it did not work with the MC1321.
bye